hid multiple endpoints

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

hid multiple endpoints

2,718件の閲覧回数
kamransial
Contributor I

Hi i am trying to make multiple endpoints using the sample code of usb hid mouse mqx k20 but only one endpoint is sending data to pc other endpoint does not initialize. i made 2 interfaces each with one endpoint and used these commands to initialize two different hid devices  

g_mouse2.app_handle = USB_Class_HID_Init(&config_struct2);

g_mouse.app_handle = USB_Class_HID_Init(&config_struct);

ラベル(2)
0 件の賞賛
返信
1 返信

1,921件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hello,

 

The HID Mouse example of MQX doesn’t include the descriptors for supporting OUT endpoints. It is required to add this support, and modify the Device and Interface descriptors, besides of adding the related Endpoint descriptors. On the following thread you will find an implementation of a Generic HID device based on the bare-metal Freescale USB Stack and a S08JS16 device. The low level implementation is almost the same for MQX and K20, so you could use it as reference:

 

https://community.freescale.com/message/320915#320915

 

Hope this will be useful for you.

Best regards!

/Carlos