frdm kl25z, problem following the Getting Started tuttorial

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

frdm kl25z, problem following the Getting Started tuttorial

ソリューションへジャンプ
1,795件の閲覧回数
MihaelF
Contributor II

Hello.

I've recenly purchased frdm-kl25z board, it is my first time working with MCU.

I'm trying to follow the Getting Started tutorial.

https://www.nxp.com/document/guide/get-started-with-the-frdm-kl25z:NGS-FRDM-KL25Z

 

On step #2 i install Tera Term, but when i try to use it as in a tutorial i don't get the x,y coordinates but that...

What may I be doing wrong?

 

Untitled.jpg

 

 

0 件の賞賛
返信
1 解決策
1,772件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Which example do you use? You can try the "hello_world' demo. It will show 'hello world' in Tera Term.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,773件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Which example do you use? You can try the "hello_world' demo. It will show 'hello world' in Tera Term.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信