Withoout S32K MCAL package

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Withoout S32K MCAL package

2,881件の閲覧回数
842203661
Contributor II

Hi, 

      I have a  S32K MCAL project base on S32K14X_MCAL4_2_RTM_1_0_1. when I import and open the project in EB  tresos, EB push error:
    Plug-in with a module "Can_TS_T40D2M10I1R0" is not installed - cannot create module configurations for project "S32K146_4.2_RTM1.0.1"

    Unfortunately, the installation package  cannot be found on the NXP official website. How do I get it?

0 件の賞賛
返信
4 返答(返信)

2,871件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

Please open your EB tresos, choose Help - EB Tresos Detail. In Bundle Registry tab, check whether the Can package was installed successfully and the path of it.

 

nxf48630_0-1600072522338.png

Regards,

Nam

0 件の賞賛
返信

2,866件の閲覧回数
842203661
Contributor II

Without packages in the window. Because I don't have  “S32K14X_MCAL4_2_RTM_1_0_1.exe”  installation package.

I already have installation packages for V1.0.0 and V1.0.4, but are lack of V1.0.1, and this is exactly what I want.

0 件の賞賛
返信

2,857件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

Your request has been processed. Please check in your Software Licensing and Support, AUTOSAR MCAL product and find in the Previous tab.

Nam

0 件の賞賛
返信

2,855件の閲覧回数
842203661
Contributor II

Wow! Nam, thank you very much! I get it.