flexio_TWR-LCD-RGB is Missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flexio_TWR-LCD-RGB is Missing

2,114件の閲覧回数
ganesan_doraisa
Contributor II

The application note AN5280 titled "Using Kinetis FlexIO to Drive a Graphical LCD" section 7.2 say to install KSDK v1.3.0 mainline release to get the flexio_TWR-LCD-RGB demo_apps directory. But the LCD project does not exist in the demo_apps folder of TWR-K80F150M within KSDK_V1.3.0. Looks like the app note says KSDK_1.3.0 comes with the project pre-installed but the KSDK does not show the project in the path listed -- C:\Freescale\KSDK_1.3.0\examples\twrk80f150m\demo_apps

タグ(1)
2 返答(返信)

1,964件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

You have the associated software here:

http://cache.nxp.com/files/archives/doc/app_note/AN5280SW.zip

Luis

1,767件の閲覧回数
richardallen2
Contributor III

Link appears down.

0 件の賞賛
返信