ezPort on Kinetis

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ezPort on Kinetis

6,952 Views
colonel_panic
Contributor I

Hi.

 

Is there a document anywhere which describes the ezPort protocol as implemented on the Kinetis family ?

 

P.

5 Replies

3,006 Views
mnorman
NXP Employee
NXP Employee

There is an EzPort chapter in the Reference Manual for each Kinetis device.  In the case of the K60 100MHz 144 pin parts, the EzPort is described in chapter 30:  K60P144M100SF2RM

 

The datasheets contain the timing specifications/requirements.  e.g. K60P144M100SF2

 

-mnorman

3,006 Views
robertofrechill
Contributor III

Hi, I´m developing the EZport programming with my Kinetis K20, I need information about what kind of file I must to charge by EZport and how I can transform my code file in this file.

Thanks.

Roberto

0 Kudos
Reply

3,006 Views
santiago_gonzal
NXP Employee
NXP Employee

Hello Roberto,

Have a look here:

Downloading an s19 file Using the

EzPORT Module on the MCF521x

ColdFire® Microcontroller.

http://www.freescale.com/files/32bit/doc/app_note/AN3897.pdf

The file you need to generate is a binary s19 file.

Regards.

0 Kudos
Reply

3,006 Views
robertofrechill
Contributor III

thanks!

Regards

0 Kudos
Reply

3,006 Views
LuisCasado
NXP Employee
NXP Employee

Hi ,

Have you seen this AN?

AN4406 
AN4406, KwikStik-based EzPort programmer - Application Notes

Luis

0 Kudos
Reply