extra SPI using FlexIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

extra SPI using FlexIO

ソリューションへジャンプ
2,056件の閲覧回数
gschelotto
Contributor V

Hi,

I have to implement 3 independent 4-wire SPI master channels on MKL17Z. Just to be sure, is it possible to do it using SPI0, SPI1 and FlexIO without constraints? If so, can I use any FlexIO port (from D0 to D7) to implement the extra SPI channel?

regards,

gaston

0 件の賞賛
返信
1 解決策
1,858件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Gaston Schelotto,

     SPI0, SPI1 and FlexIO are the different modules, so you can use these modules as SPI functions, no constraints.

    About the flexIO pin, you can use any FlexIO port to implement the extra SPI channel:

pastedImage_1.png

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,859件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Gaston Schelotto,

     SPI0, SPI1 and FlexIO are the different modules, so you can use these modules as SPI functions, no constraints.

    About the flexIO pin, you can use any FlexIO port to implement the extra SPI channel:

pastedImage_1.png

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信