extra SPI using FlexIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

extra SPI using FlexIO

Jump to solution
2,164 Views
gschelotto
Contributor V

Hi,

I have to implement 3 independent 4-wire SPI master channels on MKL17Z. Just to be sure, is it possible to do it using SPI0, SPI1 and FlexIO without constraints? If so, can I use any FlexIO port (from D0 to D7) to implement the extra SPI channel?

regards,

gaston

0 Kudos
Reply
1 Solution
1,966 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Gaston Schelotto,

     SPI0, SPI1 and FlexIO are the different modules, so you can use these modules as SPI functions, no constraints.

    About the flexIO pin, you can use any FlexIO port to implement the extra SPI channel:

pastedImage_1.png

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,966 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Gaston Schelotto,

     SPI0, SPI1 and FlexIO are the different modules, so you can use these modules as SPI functions, no constraints.

    About the flexIO pin, you can use any FlexIO port to implement the extra SPI channel:

pastedImage_1.png

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply