error [Li005] no definition for __iar_FDtest

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

error [Li005] no definition for __iar_FDtest

ソリューションへジャンプ
3,298件の閲覧回数
sourabh_vyas
Contributor I

In IAR 8.0 while compiling the code i'm getting this error

error [Li005] no definition for __iar_FDtest[referenced from MeteringRun.o(MetLibary.a)].

1 解決策
3,138件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Sourabh vyas,

    Thank you for your updated information.

    So, the problem may still be the compatibility problems between IAR7 and IAR8.

   The library may build in the IAR7, then if you use the IAR8 to include the IAR7 library, it has the problems.

   Then, if you use that MetLibary old lib, you may still need to use IAR7.

    BTW, you can share your official code link, I will help you to check whether that code still in updated support or not.


Have a great day,
kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
3,138件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi sourabh vyas,

     Please tell me what's the code you are compiling now? Is it the official code or your own code.

    It seems you lack the MetLibary.a, your project use it, but you didn't add that library.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,138件の閲覧回数
sourabh_vyas
Contributor I

Thanks for replying.

This code is official code. we are using IAR7, in that  is compiling perfectly but when we are migrating to IAR 8 it is throwing this error. This "MetLibary.a" is present in library folder.

IAR 7 is taking care but IAR 8 not.

How to resolve this thing sir. 

0 件の賞賛
返信
3,139件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Sourabh vyas,

    Thank you for your updated information.

    So, the problem may still be the compatibility problems between IAR7 and IAR8.

   The library may build in the IAR7, then if you use the IAR8 to include the IAR7 library, it has the problems.

   Then, if you use that MetLibary old lib, you may still need to use IAR7.

    BTW, you can share your official code link, I will help you to check whether that code still in updated support or not.


Have a great day,
kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------