disabled the watchdog timer, but reset by the watchdog timer.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

disabled the watchdog timer, but reset by the watchdog timer.

跳至解决方案
3,659 次查看
jun1
Contributor V

Please kindly advise.

I have disabled the watchdog timer, but it seems to be reset by the watchdog timer.
The following sources. I am using SDK_2.6.0_MKE04Z128xxx4.

Disable the watchdog timer.


  WDOG8_GetDefaultConfig (& wdogConfig);
  wdogConfig.timeoutValue = WDOG_TIMEOUT;
  wdogConfig.enableInterrupt = true;
  wdogConfig.enableWdog8 = false;      // for debug
  WDOG8_Init (WDOG, & wdogConfig);

 

So, at startup, check with the following function at the beginning.
bool boardResetWDT (void)
{
  uint32_t bl = SIM_SRSID_WDOG (1);
  uint32_t srsid = (SIM-> SRSID);
.
  if ((bl & srsid)! = 0u) {  // 1 Reset caused by WDT
    return true;
  }
  return false;
}


Then it will return true.

I left it unattended and restarted surely, so I was investigating whether the watchdog was the cause, but even if I disabled it, it restarted and it seems that the watchdog is the cause, but what is happening? Is not it?
Is there anything other than the watch dock that causes the reboot?

Thank you.

 

jun.

 

 

 

0 项奖励
回复
1 解答
3,629 次查看
jun1
Contributor V

Hi.

solved.

It seems that it was reset because the watchdog timer was not cleared within 16 cycles (an interrupt was inserted in between). After clearing the watchdog timer in the interrupt disabled state, the reset no longer occurs.

Thank you very much.


jun.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,634 次查看
nxf58904
NXP Employee
NXP Employee

Hi,

Have you enabled the watchdog  before you disable the wadg?

Can you refer this link to check if wdg went to wdg_handle.https://community.nxp.com/t5/Kinetis-Microcontrollers/disabled-the-watchdog-timer-but-reset-by-the-w....

And can you debug to check if WDOG_CS1.7 has been set  after you disabled the wdg.

33333333333333333333.png

 

 

Jianyu: 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
3,630 次查看
jun1
Contributor V

Hi.

solved.

It seems that it was reset because the watchdog timer was not cleared within 16 cycles (an interrupt was inserted in between). After clearing the watchdog timer in the interrupt disabled state, the reset no longer occurs.

Thank you very much.


jun.

0 项奖励
回复