could not find core in coresight setup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

could not find core in coresight setup

15,150 次查看
albertdoe
Contributor I

Using Segger J-Flash v6.32g, processor MK22FN1M0VLH12. J-Flash Target Connect shows (in the log)

Connecting ...
 - Connecting via USB to J-Link device 0
 - Target interface speed: 4000 kHz (Fixed)
 - VTarget = 3.325V
 - ERROR: Could not find core in Coresight setup
 - ERROR: Failed to connect.
Could not establish a connection to target.

标记 (1)
0 项奖励
回复
2 回复数

11,924 次查看
tbiberdorf
Contributor IV

Hi Jing:

I'm using a K60DN512VLL10 and I encountered the same "could not find core in coresight setup" problem.

I'm using Segger V6.56B

I connected with J-Link Commander V6.56b to attempt to unlock my core as suggested by Jing, and the command tool is unable to connect.

It appears to unlock with success but cannot erase.  It encounters the same problem:Could not find core in Coresight setup.

Can you provide other suggestions? 

pastedImage_1.png

0 项奖励
回复

11,924 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Albert,

If there is no other hardware issue, I guess your chip is locked. Please see this link:

https://community.nxp.com/message/1013892 

Regards,

Jing

0 项奖励
回复