could not find core in coresight setup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

could not find core in coresight setup

16,728 Views
albertdoe
Contributor I

Using Segger J-Flash v6.32g, processor MK22FN1M0VLH12. J-Flash Target Connect shows (in the log)

Connecting ...
 - Connecting via USB to J-Link device 0
 - Target interface speed: 4000 kHz (Fixed)
 - VTarget = 3.325V
 - ERROR: Could not find core in Coresight setup
 - ERROR: Failed to connect.
Could not establish a connection to target.

0 Kudos
Reply
2 Replies

13,501 Views
tbiberdorf
Contributor IV

Hi Jing:

I'm using a K60DN512VLL10 and I encountered the same "could not find core in coresight setup" problem.

I'm using Segger V6.56B

I connected with J-Link Commander V6.56b to attempt to unlock my core as suggested by Jing, and the command tool is unable to connect.

It appears to unlock with success but cannot erase.  It encounters the same problem:Could not find core in Coresight setup.

Can you provide other suggestions? 

pastedImage_1.png

0 Kudos
Reply

13,501 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Albert,

If there is no other hardware issue, I guess your chip is locked. Please see this link:

https://community.nxp.com/message/1013892 

Regards,

Jing

0 Kudos
Reply