converter from CAN to UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

converter from CAN to UART

3,454件の閲覧回数
kentgu
Contributor III

hi, If Freescal have one chip, can realize convter CAN bus to UART, it don' need to program. TKS~ Kent

0 件の賞賛
返信
2 返答(返信)

2,454件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Kent,

Please go ahead to find some information about the CAN transceivers through the link as below.

CAN Physical Interfaces|Freescale
Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,454件の閲覧回数
kentgu
Contributor III

Hi Jerremy,

Yes, you are right. we can use CAN transciever. but it just realize to CANRx, CANTx signal to differentiial signal. can't convert CAN protocol to UART protco..

TKS~

Kent

0 件の賞賛
返信