clock configuration for K60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

clock configuration for K60

1,774件の閲覧回数
mehdikarimibiuk
Contributor V

I am having a bareboard project with processor expert with added several components in it.

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,507件の閲覧回数
apanecatl
Senior Contributor II

Since you are using FBE, the FLL IS NOT providing the core clock since it is being bypassed as per the MCG mode indicates. Your core is running at the XTAL frequency, which in this case is 16MHz; to run at 100MHz you would have to use FEE with the same configuration.

0 件の賞賛
返信

1,507件の閲覧回数
pascalschröer
Contributor V

That's my question too -.- hope anyone can solve this question^^

greets

0 件の賞賛
返信