clock configuration for K60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

clock configuration for K60

1,787 Views
mehdikarimibiuk
Contributor V

I am having a bareboard project with processor expert with added several components in it.

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

1,520 Views
apanecatl
Senior Contributor II

Since you are using FBE, the FLL IS NOT providing the core clock since it is being bypassed as per the MCG mode indicates. Your core is running at the XTAL frequency, which in this case is 16MHz; to run at 100MHz you would have to use FEE with the same configuration.

0 Kudos
Reply

1,520 Views
pascalschröer
Contributor V

That's my question too -.- hope anyone can solve this question^^

greets

0 Kudos
Reply