choose Cortex M4 fro medical device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

choose Cortex M4 fro medical device

1,961件の閲覧回数
avihookeret1
Contributor I

for medical device ( 7 years of manufacture )  can you recommend me for Cortex m4 small footprint CPU

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,881件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.

I was wondering if you can share the more detailed requirements about the MCU.

After get the information, I think I can have the better suggestion for you.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,881件の閲覧回数
avihookeret1
Contributor I

--

Best Regards,

Avi Keret

ToucheMedical Ltd

0 件の賞賛
返信

1,881件の閲覧回数
avihookeret1
Contributor I

Dear Ping

We are looking for:

Project 1: medical device

1. Longevity Program 10 years

2. Small size <= 5x5 mm

3. ARM cortex M0 M3 or M4

4. Flash size 16, 32 K

5. Ram 2K and 4K

6. Io > 16

7. 1 A2D 12 bit or more

8. Local oscillator

9.

Project 2: medical device

1. Longevity Program 10 years

2. Small size <= 5x5 mm

3. ARM cortex M4

4. Flash size 64, 128 K

5. Ram 8K and 16K

6. Io > 22

7. 1 A2D 12 bit or more 4 inputs

8. Local oscillator

9. Small size 128*128 pixels screen

10.

--

Best Regards,

Avi Keret

ToucheMedical Ltd

0 件の賞賛
返信