can't set security of kl05z32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can't set security of kl05z32

Jump to solution
2,486 Views
wangbaode
Contributor IV

Dear ,

I want to secure my chip through Flash configuration field in kl05z32.but I'm failed.

I define many constant variable in Flash configuration field.But I find the data can't writen into flash through cw10.3.

6134_6134.pngpastedImage_0.png

 

my project is in attachment .

 

best regards

Original Attachment has been moved to: KL05Z32_Security.rar

Tags (2)
0 Kudos
Reply
1 Solution
2,347 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Baode,

That is becase you try to secure the KL device, so that the Jlink will stop you in that case. Actually it is not recommend to secure the device if you still want to debug the application as debug is not supported on a secured device. so in debug phase, you may just set FSEC as 0x02, and in factory phase, turn it to 0x00. Please note to use the OpenSDA to download the secured image into device instead of Jlink.

Hope that helps,

B.R

Kan

View solution in original post

0 Kudos
Reply
8 Replies
2,347 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

I have reviewed your project as well as the map file, they look fine, but when I tried to download the image into FRDM-KL05Z with the help of CW 10.4, the connection failed anyway, so I have to open a released KL05 project in the same workspace, for example, KL05_Freedom_Demo_cw as below,

2.png

and choose the connection type from that demo:

3.png

The download passed successfully and you may see the Flash configuration field was modified as you expected.

1.png

Hope that helps,

B.R

Kan

2,347 Views
wangbaode
Contributor IV

Dear Kan_Li,

you're right. in my project, I use BDM to debug.Now I use Jlink to debug the project and I also can see data is in flash. I think it's a bug of usbdm.

pastedImage_0.png

But another question comes out.

I watch the register of flash controller.I find the register don't be updated by data in flash configuration field.

In reference,

pastedImage_0.png

data in 0x40D is 0x00,But value in FOPT register is 0xff.

Why?

0 Kudos
Reply
2,347 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Baode,

How did you confirm the value in FOPT register? Using the CW's register viewer? If you look into this via CW's viewer immediately after downloading the image, the FOPT is what before program. It is recommended to use the printf() fucntion to watch the updated value after a POR on this device.

Hope that helps,

B.R

Kan

2,347 Views
wangbaode
Contributor IV

Hi Kan,

I watch the value via CW's register viewer after downloading this image.

according to your suggestion,I use the printf() fucntion to watch the value and I find the value is the same as

the register viewer.

pastedImage_0.png

pastedImage_1.png

pastedImage_2.png

0 Kudos
Reply
2,347 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Baode,

Did you disconnect the JTAG and KL05 device after downloading and power off and re-power on the device to run the embedded application? Please kindly help to clarify. Thanks for your patience!!

B.R

Kan

0 Kudos
Reply
2,347 Views
wangbaode
Contributor IV

Hi Kan,

Thans for your patience. according to your suggestion,after i download my program and re-power on the device,I program my program again and i can see the value in register viewer and control consle.

pastedImage_1.png

But when i set FSEC as 0x00 and debug the program, codewarrior give me a warning dialog as follow.

pastedImage_2.png

How to configure my project to remove the dialog?

0 Kudos
Reply
2,348 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Baode,

That is becase you try to secure the KL device, so that the Jlink will stop you in that case. Actually it is not recommend to secure the device if you still want to debug the application as debug is not supported on a secured device. so in debug phase, you may just set FSEC as 0x02, and in factory phase, turn it to 0x00. Please note to use the OpenSDA to download the secured image into device instead of Jlink.

Hope that helps,

B.R

Kan

0 Kudos
Reply
2,347 Views
wangbaode
Contributor IV

Hi Kan,

Thanks.I see you.

Bye

0 Kudos
Reply