can ripple mixed in power pin cause mcu resets?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

can ripple mixed in power pin cause mcu resets?

1,148 次查看
wangbaode
Contributor IV

hi everybody,

can ripple mixed in power pin cause mcu(kl15z128) resets? and how many is the threshold of ripple voltage?

best regards for everyone

标记 (5)
0 项奖励
回复
2 回复数

973 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Bao De

What is your ripple range? 0.5V? Do you enable LVD function? If yes, please check which LVD level you selected. As you know, VLVW4H max. value is 3.08V. Waiting for your response. Thanks

Best Regards

Paul

0 项奖励
回复

973 次查看
mjbcswitzerland
Specialist V

Hi

The data sheet to the devices give the lowest operating voltage and I would expect that if any power supply ripple stays above that things would be OK.

In case you have resets that "may" be caused due to this, read the RCM_SRS0 register after a reset to see whether it was due to a "power on reset" or "low voltage detector" or possibly another reason.

Regards

Mark

0 项奖励
回复