blhost doesnt allow recognize few Kinetis devices connected to host by USB HID. As blhost use only USB VID and USB PID params wich doesnt allow to adress few devices., blhost doesnt allow recognize few Kinetis devices connected to host by USB HID. As blho

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

blhost doesnt allow recognize few Kinetis devices connected to host by USB HID. As blhost use only USB VID and USB PID params wich doesnt allow to adress few devices., blhost doesnt allow recognize few Kinetis devices connected to host by USB HID. As blho

1,985件の閲覧回数
vyacheslavguzhv
NXP Employee
NXP Employee

blhost doesnt allow recognize few Kinetis devices connected to host by USB HID. As blhost use only USB VID and USB PID params wich doesnt allow to adress few devices.

Please suggest if there is updated version for blhost with fixed issue or if its possible to get sources of blhost

0 件の賞賛
返信
4 返答(返信)

1,891件の閲覧回数
vyacheslavguzhv
NXP Employee
NXP Employee

in case there is no workaround, would it be possible to make Change Request for future version of blhost in order to support such feature?

thanks!

Slava

0 件の賞賛
返信

1,891件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

I can't find any way to get around except plus and plug. I'm afraid there won't be any change if there is future version, since your application is very unique. I think you have to make your own blhost.

Regards,

Jing

0 件の賞賛
返信

1,891件の閲覧回数
vyacheslavguzhv
NXP Employee
NXP Employee

hello!

thanks for explanations! Yes, i need to manage few connected Kinetis devices at once with USB HID.

What can yopu recomend as the workaround for my case?

Slava

0 件の賞賛
返信

1,891件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

I am a bit confused about your question. First, blhost source code is not open to customer. And you said " blhost use only USB VID and USB PID params which doesn't allow to address few devices". Yes, blhost use VID and PID to identify the device. But you can change default VID and PID.

Do you mean you want to connect two board with same VID/PID to computer and download at same time? No, it does't work. It seems blhost can't operate multi board with a single command.

Regards,

Jing

0 件の賞賛
返信