bin to hex conversion

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bin to hex conversion

20,116件の閲覧回数
fabrizioefm
Contributor II

Hello everyone, I have to convert a .bin file to one .hex. Can anyone tell me how I can do? thank you and greetings. Fabrizio

0 件の賞賛
返信
9 返答(返信)

17,771件の閲覧回数
fabrizioefm
Contributor II

thanks, these are all good solutions!

Regards

Fabrizio

0 件の賞賛
返信

17,771件の閲覧回数
Ray_V
Contributor V

As Philippe GRAILLE mentioned, if you are using MCUXpresso it can create the Hex file for you.
To do this automatically you can go in the settings and add the following to the post-build steps.

arm-none-eabi-objcopy -v -O ihex "${BuildArtifactFileName}" "${BuildArtifactFileBaseName}.hex"

if you prefer the MOTOROLA SRECORD format, use:

arm-none-eabi-objcopy -v -O srec "${BuildArtifactFileName}" "${BuildArtifactFileBaseName}.srec"

Converting from binary can be tricky as the binary files have no address location information.

So, if your code does not start at address 0, you need a tool where you can specify the memory location when converting.

0 件の賞賛
返信

17,771件の閲覧回数
mjbcswitzerland
Specialist V


Hi

See also the utilities in the uTasker project: http://www.utasker.com/forum/index.php?topic=1445.0

These allow flexible ways to convert between formats, combine boot and application files, or generate arrays based on images, web pages etc. for embedding into code or embedding code that is to be uploaded to other processors into code. The collection had been developed over 14 years of real project requirements so contains most of what embedded programmers need to be able to do in varied situations.

There is also support for Motorola binary format (output from older CW IDEs) or encrypting and authenticating applications for use by secure boot loaders.

Regards

Mark

0 件の賞賛
返信

17,771件の閲覧回数
stephenmcintyre
Contributor II

use bin2hex.exe on windows. There is similar tools available for post build conversion on Linux.

Hope this helps

0 件の賞賛
返信

17,771件の閲覧回数
gph
Contributor III

Hi,

In MCUXpresso :

   Right click on your binary axf file

      Binary Utility / Create HEX

In command line :

   arm-none-eabi-objcopy  -O binary "${FileName}" "${FileBaseName}.bin"

Philippe.

0 件の賞賛
返信

17,771件の閲覧回数
fabrizioefm
Contributor II

Hi Erich,

my problem is this: I'm using the application CreateImage (of PEMICRO) to create the image of my KEA128 kinetis firmware, using Cyclone FX. My firmware consists of two blocks, bootloader + application. Since CreateImage does not accept .bin formats it only accepts HEX formats, so I used an application, HexEdit 4.0 (I do not know if you know it) to export the file in Srec format (S2 Motorola record). I have just discovered, however, that when it generates this format the checksum is wrong, increasing the correct value by 1.
for example the record line:
S2240004000000000000000000FFFFFFFF82FFFFFF10B58A18914210D00302000A0C78034369 ends with 69 but the exact checksum is 68.
In practice, each record line ends with a value of +1 relative to the correct value.
That is why Cyclone FX rightly gives ERROR VERIFY.

The application that tips works correctly? does it also exist to convert Srec motorola format?
Thank you

Fabrizio

0 件の賞賛
返信

17,771件の閲覧回数
Ray_V
Contributor V

S record uses the 1's complement of the lower byte of the sum of all bytes, not the 2's complement as Intel Hex does.

The 2 in S2 is not part of the checksum. So 69 is the correct checksum for this S record.

17,771件の閲覧回数
fabrizioefm
Contributor II

my operating system is win 64bit...

0 件の賞賛
返信

17,771件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Fabrizio,

Converting Binary Files to Intel Hex Format with the SRecord Tool | MCU on Eclipse  should be what you are asking for?

I hope this helps,

Erich

0 件の賞賛
返信