arm-none-eabi-gdb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

arm-none-eabi-gdb

5,050件の閲覧回数
tahirmahmood
Contributor I

I am getting the following error  when I do RUN->Debug.How can I get rid of this error.

Error while launching command: arm-none-eabi-gdb --version

0 件の賞賛
返信
5 返答(返信)

3,958件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Tahir,

Could you tell us which MCU and IDE are you using?

Thanks in advance!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信

3,958件の閲覧回数
tahirmahmood
Contributor I

Hello Mendoza,

One additional thing is that I am getting this problem with Segger J-link.

Mit freundlichen Grüßen / Best Regards

Tahir Mahmood

MSc.

Entwicklung Elektronik

Von: Carlos_Mendoza

Gesendet: Montag, 30. Mai 2016 17:42

An: Mahmood, Tahir

Betreff: Re: - arm-none-eabi-gdb

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

arm-none-eabi-gdb

reply from Carlos_Mendoza<https://community.nxp.com/people/Carlos_Mendoza?et=watches.email.thread> in Kinetis Microcontrollers - View the full discussion<https://community.nxp.com/message/655648?et=watches.email.thread#comment-655648>

0 件の賞賛
返信

3,958件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Tahir,

Thanks for your response. Please make sure that the correct connection is selected on the debug configurations:

pastedImage_0.png

pastedImage_1.png

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,958件の閲覧回数
amuresan
Contributor III

This is not helpful. At all. Have you even tested this solution?

I have the exact same problem after correctly selecting SEGGER. 

YOU HAVE A BUG. FIX IT.

0 件の賞賛
返信

3,958件の閲覧回数
tahirmahmood
Contributor I

Hello Mendoza,

I am using MK10DN128VFM5 with KDS 3.0.0. I am using my own tool chain.

Mit freundlichen Grüßen / Best Regards

Tahir Mahmood

MSc.

Entwicklung Elektronik

Von: Carlos_Mendoza

Gesendet: Montag, 30. Mai 2016 17:42

An: Mahmood, Tahir

Betreff: Re: - arm-none-eabi-gdb

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

arm-none-eabi-gdb

reply from Carlos_Mendoza<https://community.nxp.com/people/Carlos_Mendoza?et=watches.email.thread> in Kinetis Microcontrollers - View the full discussion<https://community.nxp.com/message/655648?et=watches.email.thread#comment-655648>

0 件の賞賛
返信