alphanumeric display and sd card support on k70

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

alphanumeric display and sd card support on k70

1,191件の閲覧回数
sivakamasundari
Contributor I

do you have  alpha numeric keypad interface driver support on k70 platform (bare metal coding)?

if not kindly suggest how it can be done?

do u have sd card support using filesystem in k70 platform?

pl support on bare metal code  with file system for sd card interface and alpha numeric display

0 件の賞賛
返信
1 返信

1,112件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

The Secure Digital Host Controller (SDHC) module included on Kinetis supports the specification version 2.0 of SDCard.org; this specification supports SD Cards up to 32 GB. You can find this at the SDHC chapter of the K70’s Reference Manual.

As for the alpha numeric keypad, K70 do not support it directly but we had provide an GPIO expander which make this available.

http://cache.nxp.com/documents/leaflet/75016987.pdf?fsrch=1&sr=1&pageNum=1 

0 件の賞賛
返信