a simple example of ethernet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

a simple example of ethernet

3,173件の閲覧回数
Kam
Contributor I

Hi

        I need a simple example of ethernet. My project just need the ethernet  module send or receive a MAC frame and no need the tcp/ip  protocol stack. I study "freertos_lwip","freertos_uip" and "MQX". Think that too complex to i can't understand. Could i get some document or UM about it ? And  it's well if i can get a simple example. Thank you.

0 件の賞賛
返信
1 返信

2,116件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

The K60's Ethernet controller has a compatibility mode for backward compatibility the Coldfire Ethernet module. Therefore you can also use any old Coldfire Ethernet driver code as an example.

 

If you are using the Tower kit you will however need to ensure that the PHY's 50MHz clock is selected (it needs RMII mode) and that this is routed over the backplane to the processor (for use as clock) since both clocks need to be synchronised for operation - see also section 7 of http://www.utasker.com/docs/KINETIS/uTaskerV1.4_Kinetis_demo.pdf

 

Regards

 

Mark

 

0 件の賞賛
返信