a simple example of ethernet

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

a simple example of ethernet

2,605 次查看
Kam
Contributor I

Hi

        I need a simple example of ethernet. My project just need the ethernet  module send or receive a MAC frame and no need the tcp/ip  protocol stack. I study "freertos_lwip","freertos_uip" and "MQX". Think that too complex to i can't understand. Could i get some document or UM about it ? And  it's well if i can get a simple example. Thank you.

0 项奖励
回复
1 回复

1,548 次查看
mjbcswitzerland
Specialist V

Hi

 

The K60's Ethernet controller has a compatibility mode for backward compatibility the Coldfire Ethernet module. Therefore you can also use any old Coldfire Ethernet driver code as an example.

 

If you are using the Tower kit you will however need to ensure that the PHY's 50MHz clock is selected (it needs RMII mode) and that this is routed over the backplane to the processor (for use as clock) since both clocks need to be synchronised for operation - see also section 7 of http://www.utasker.com/docs/KINETIS/uTaskerV1.4_Kinetis_demo.pdf

 

Regards

 

Mark

 

0 项奖励
回复