Write/Read on SD Card without filesystem (Raw Data)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Write/Read on SD Card without filesystem (Raw Data)

4,201件の閲覧回数
juancamilomonto
Contributor I

Hello,

Im looking for a project to write and read data on an SD Card without using FatFs, only raw data.

I need to write some information and later read it to show it using UART.

thanks a lot.

Juan Camilo Montoya

タグ(3)
0 件の賞賛
返信
1 返信

2,660件の閲覧回数
mjbcswitzerland
Specialist V

Hello

Any file system implementation will be based on a driver interface (for SDHC or SPI) that reads and writes SD card sectors (512 bytes in size).

This means that you can take any such implementation and directly call these sector read and write routines to read or write the (raw) sectors.

If you load any of the references at µTasker Kinetis support containing the SD card interface (ufFAT2.0) there is also a direct sector interface that can be accessed in the disk drive menu "sect" allows a sector to be read and "sectw" allows a sector to be written.

Regards

Mark

Kinetis: µTasker Kinetis support

utFAT2.0: http://www.utasker.com/docs/uTasker/uTasker_utFAT.PDF

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 件の賞賛
返信