Will the K12 gain KSDK 2.0 support?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Will the K12 gain KSDK 2.0 support?

Jump to solution
1,617 Views
jacobjennings
Contributor III

Will K12 get KDS / KSDK 2.0 support?

Thanks,

Jake

Labels (1)
0 Kudos
Reply
1 Solution
1,512 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Jacob,

The K12 50MHz is during field trial phase.

And haven't receive the information about when it will release.

K12 50MHz KSDK2.0.jpg

Best Regards,

Robin

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,513 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Jacob,

The K12 50MHz is during field trial phase.

And haven't receive the information about when it will release.

K12 50MHz KSDK2.0.jpg

Best Regards,

Robin

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------