Converting from KL43 to KL17 project KDS KSDK 2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Converting from KL43 to KL17 project KDS KSDK 2.0

847 Views
ken_sloat
Contributor II

We've been developing an application on a FRDM-KL43Z board but now want to port it to our custom board with a KL17. I notice that the driver set for the two is nearly identical with the exception of a line in the clocks about USB. Is it necessary to convert the project, and if so how do we properly do this?

0 Kudos
Reply
1 Reply

745 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Kenneth,

Do you said the kl17256?

If yes, yes ,you can download the project about frdm-kl43 into kl17.

While i recommend you create one project on KDS about KL17, then copy

the application code on kl43 board in to the project , then download it .

Hope it helps

Alice

0 Kudos
Reply