Why is my application intermittently failing to start properly when being loaded by a bootloader?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why is my application intermittently failing to start properly when being loaded by a bootloader?

3,834 次查看
aaronledger
Contributor I

I am using the K22FN1M0 part and having an issue where a small number of processors seem to be affected. The problem is that sometimes, the main application seems to fail to run properly intermittently. The same exact code will run on other parts seemingly just fine. When I say fails to run properly, I mean we get behavior as if it were some unhandled exception. If the code is slightly altered and recompiled, the processors that were failing may behave as expected. I'm looking for some ideas about how to troubleshoot this further.

I am using a custom bootloader that essentially does the following:

    __disable_irq();

    uint32_t new_sp = IMAGE_ADDR[0];

    uint32_t new_pc = IMAGE_ADDR[1];

    SCB->VTOR = (uint32_t)BLOCK1_BASE;

    asm("mov LR, 0xFFFFFFFF");

    __set_MSP(new_sp);

    __set_PSP(new_sp);

    ((void(*)(void))new_pc)();

In this case, IMAGE_ADDR is the 2nd flash block (also BLOCK1_BASE) where the main application is located. Note that the processor startup code is shared in both main application and bootloader. Before utilizing a bootloader, this type of issue was not observed. I have altered the main application to not run some of the startup code that is already run by the bootloader, but it had no affect on the issue. Are there certain items in startup that if run a second time could result in some behavior like this? Any insight is appreciated.

标签 (1)
0 项奖励
回复
5 回复数

2,948 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Aaron Ledger,

Would you please tell us which boot loader you are using , and the version info? is it a custom boot loader? Please kindly help to clarify.

Thanks for your patience!

Kan

0 项奖励
回复

2,948 次查看
mjbcswitzerland
Specialist V

Aaron

When your boot loader completes its work (also when not actually loading anything) have you verified that all peripherals and interrupts that it enabled are disabled?

I work a lot with boot loaders and have occasionally had effects where occasionally a spurious interrupt is received at the application. Even with the same software it can seem fine for some time and then suddenly do it.

Recently I had this case:

- the boot loader uses SYSTICK

- the application uses the low power timer for its TICK and doesn't enabe the SYSTICK or its interrupts in the NVIC

- occasionally I has a case where there was a spurious interrupt

- I found that writes to the NVIC used to disable all previously used interrupts by the loader were operating normally for the peripherals but I could see that the SYSTICK flags were "sticking". Not understanding why, I disabled the SYSTICK instead and this solved the issue.

It may be worth setting a break point at the jump from loader to application and checking through all interrupt registers to see whether something is pending/enabled. This is how I saw that there was something in thixs case that obviously could sometimes cause problems. It is also when I found that the SYSTICK masks in the NVIC (which I thought had been cleared) were sticking because I couldn't set them back with the debugger either (???).

Regards

Mark

Kinetis: µTasker Kinetis support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 项奖励
回复

2,948 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Aaron Ledger,

What did you do in your startup()? would you please share it for a review? and what do you mean the shared startup()? do boot loader and application call this startup() via a unique entry? Please kindly help to clarify. Thanks for your patience!


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,948 次查看
aaronledger
Contributor I

Here is the startup code being used. When I say shared, I mean that both the bootloader and then the main application run through the same startup routines below, however, I have defined __NO_SYSTEM_INIT for the main application.

/* ---------------------------------------------------------------------------------------*/

/*  @file:    startup_MK22F12.s                                                           */

/*  @purpose: CMSIS Cortex-M4 Core Device Startup File                                    */

/*            MK22F12                                                                     */

/*  @version: 1.7                                                                         */

/*  @date:    2014-2-18                                                                   */

/*  @build:   b140606                                                                     */

/* ---------------------------------------------------------------------------------------*/

/*                                                                                        */

/* Copyright (c) 1997 - 2014 , Freescale Semiconductor, Inc.                              */

/* All rights reserved.                                                                   */

/*                                                                                        */

/* Redistribution and use in source and binary forms, with or without modification,       */

/* are permitted provided that the following conditions are met:                          */

/*                                                                                        */

/* o Redistributions of source code must retain the above copyright notice, this list     */

/*   of conditions and the following disclaimer.                                          */

/*                                                                                        */

/* o Redistributions in binary form must reproduce the above copyright notice, this       */

/*   list of conditions and the following disclaimer in the documentation and/or          */

/*   other materials provided with the distribution.                                      */

/*                                                                                        */

/* o Neither the name of Freescale Semiconductor, Inc. nor the names of its               */

/*   contributors may be used to endorse or promote products derived from this            */

/*   software without specific prior written permission.                                  */

/*                                                                                        */

/* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND        */

/* ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED          */

/* WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE                 */

/* DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE FOR       */

/* ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES         */

/* (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES;           */

/* LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON         */

/* ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT                */

/* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS          */

/* SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.                           */

/*****************************************************************************/

/* Version: GCC for ARM Embedded Processors                                  */

/*****************************************************************************/

    .syntax unified

    .arch armv7-m

    .section .isr_vector, "a"

    .align 2

    .globl __isr_vector

__isr_vector:

    .long   __StackTop                                      /* Top of Stack */

    .long   Reset_Handler                                   /* Reset Handler */

    .long   NMI_Handler                                     /* NMI Handler*/

    .long   HardFault_Handler                               /* Hard Fault Handler*/

    .long   MemManage_Handler                               /* MPU Fault Handler*/

    .long   BusFault_Handler                                /* Bus Fault Handler*/

    .long   UsageFault_Handler                              /* Usage Fault Handler*/

    .long   0                                               /* Reserved*/

    .long   0                                               /* Reserved*/

    .long   0                                               /* Reserved*/

    .long   0                                               /* Reserved*/

    .long   SVC_Handler                                     /* SVCall Handler*/

    .long   DebugMon_Handler                                /* Debug Monitor Handler*/

    .long   0                                               /* Reserved*/

    .long   PendSV_Handler                                  /* PendSV Handler*/

    .long   SysTick_Handler                                 /* SysTick Handler*/

                                                            /* External Interrupts*/

    .long   DMA0_IRQHandler                                 /* DMA Channel 0 Transfer Complete*/

    .long   DMA1_IRQHandler                                 /* DMA Channel 1 Transfer Complete*/

    .long   DMA2_IRQHandler                                 /* DMA Channel 2 Transfer Complete*/

    .long   DMA3_IRQHandler                                 /* DMA Channel 3 Transfer Complete*/

    .long   DMA4_IRQHandler                                 /* DMA Channel 4 Transfer Complete*/

    .long   DMA5_IRQHandler                                 /* DMA Channel 5 Transfer Complete*/

    .long   DMA6_IRQHandler                                 /* DMA Channel 6 Transfer Complete*/

    .long   DMA7_IRQHandler                                 /* DMA Channel 7 Transfer Complete*/

    .long   DMA8_IRQHandler                                 /* DMA Channel 8 Transfer Complete*/

    .long   DMA9_IRQHandler                                 /* DMA Channel 9 Transfer Complete*/

    .long   DMA10_IRQHandler                                /* DMA Channel 10 Transfer Complete*/

    .long   DMA11_IRQHandler                                /* DMA Channel 11 Transfer Complete*/

    .long   DMA12_IRQHandler                                /* DMA Channel 12 Transfer Complete*/

    .long   DMA13_IRQHandler                                /* DMA Channel 13 Transfer Complete*/

    .long   DMA14_IRQHandler                                /* DMA Channel 14 Transfer Complete*/

    .long   DMA15_IRQHandler                                /* DMA Channel 15 Transfer Complete*/

    .long   DMA_Error_IRQHandler                            /* DMA Error Interrupt*/

    .long   MCM_IRQHandler                                  /* Normal Interrupt*/

    .long   FTFE_IRQHandler                                 /* FTFE Command complete interrupt*/

    .long   Read_Collision_IRQHandler                       /* Read Collision Interrupt*/

    .long   LVD_LVW_IRQHandler                              /* Low Voltage Detect, Low Voltage Warning*/

    .long   LLW_IRQHandler                                  /* Low Leakage Wakeup*/

    .long   Watchdog_IRQHandler                             /* WDOG Interrupt*/

    .long   Reserved39_IRQHandler                           /* Reserved Interrupt 39*/

    .long   I2C0_IRQHandler                                 /* I2C0 interrupt*/

    .long   I2C1_IRQHandler                                 /* I2C1 interrupt*/

    .long   SPI0_IRQHandler                                 /* SPI0 Interrupt*/

    .long   SPI1_IRQHandler                                 /* SPI1 Interrupt*/

    .long   I2S0_Tx_IRQHandler                              /* I2S0 transmit interrupt*/

    .long   I2S0_Rx_IRQHandler                              /* I2S0 receive interrupt*/

    .long   Reserved46_IRQHandler                           /* Reserved interrupt 46*/

    .long   UART0_RX_TX_IRQHandler                          /* UART0 Receive/Transmit interrupt*/

    .long   UART0_ERR_IRQHandler                            /* UART0 Error interrupt*/

    .long   UART1_RX_TX_IRQHandler                          /* UART1 Receive/Transmit interrupt*/

    .long   UART1_ERR_IRQHandler                            /* UART1 Error interrupt*/

    .long   UART2_RX_TX_IRQHandler                          /* UART2 Receive/Transmit interrupt*/

    .long   UART2_ERR_IRQHandler                            /* UART2 Error interrupt*/

    .long   UART3_RX_TX_IRQHandler                          /* UART3 Receive/Transmit interrupt*/

    .long   UART3_ERR_IRQHandler                            /* UART3 Error interrupt*/

    .long   ADC0_IRQHandler                                 /* ADC0 interrupt*/

    .long   CMP0_IRQHandler                                 /* CMP0 interrupt*/

    .long   CMP1_IRQHandler                                 /* CMP1 interrupt*/

    .long   FTM0_IRQHandler                                 /* FTM0 fault, overflow and channels interrupt*/

    .long   FTM1_IRQHandler                                 /* FTM1 fault, overflow and channels interrupt*/

    .long   FTM2_IRQHandler                                 /* FTM2 fault, overflow and channels interrupt*/

    .long   CMT_IRQHandler                                  /* CMT interrupt*/

    .long   RTC_IRQHandler                                  /* RTC interrupt*/

    .long   RTC_Seconds_IRQHandler                          /* RTC seconds interrupt*/

    .long   PIT0_IRQHandler                                 /* PIT timer channel 0 interrupt*/

    .long   PIT1_IRQHandler                                 /* PIT timer channel 1 interrupt*/

    .long   PIT2_IRQHandler                                 /* PIT timer channel 2 interrupt*/

    .long   PIT3_IRQHandler                                 /* PIT timer channel 3 interrupt*/

    .long   PDB0_IRQHandler                                 /* PDB0 Interrupt*/

    .long   USB0_IRQHandler                                 /* USB0 interrupt*/

    .long   USBDCD_IRQHandler                               /* USBDCD Interrupt*/

    .long   Reserved71_IRQHandler                           /* Reserved interrupt 71*/

    .long   DAC0_IRQHandler                                 /* DAC0 interrupt*/

    .long   MCG_IRQHandler                                  /* MCG Interrupt*/

    .long   LPTimer_IRQHandler                              /* LPTimer interrupt*/

    .long   PORTA_IRQHandler                                /* Port A interrupt*/

    .long   PORTB_IRQHandler                                /* Port B interrupt*/

    .long   PORTC_IRQHandler                                /* Port C interrupt*/

    .long   PORTD_IRQHandler                                /* Port D interrupt*/

    .long   PORTE_IRQHandler                                /* Port E interrupt*/

    .long   SWI_IRQHandler                                  /* Software interrupt*/

    .long   SPI2_IRQHandler                                 /* SPI2 Interrupt*/

    .long   UART4_RX_TX_IRQHandler                          /* UART4 Receive/Transmit interrupt*/

    .long   UART4_ERR_IRQHandler                            /* UART4 Error interrupt*/

    .long   UART5_RX_TX_IRQHandler                          /* UART5 Receive/Transmit interrupt*/

    .long   UART5_ERR_IRQHandler                            /* UART5 Error interrupt*/

    .long   CMP2_IRQHandler                                 /* CMP2 interrupt*/

    .long   FTM3_IRQHandler                                 /* FTM3 fault, overflow and channels interrupt*/

    .long   DAC1_IRQHandler                                 /* DAC1 interrupt*/

    .long   ADC1_IRQHandler                                 /* ADC1 interrupt*/

    .long   I2C2_IRQHandler                                 /* I2C2 interrupt*/

    .long   CAN0_ORed_Message_buffer_IRQHandler             /* CAN0 OR'd message buffers interrupt*/

    .long   CAN0_Bus_Off_IRQHandler                         /* CAN0 bus off interrupt*/

    .long   CAN0_Error_IRQHandler                           /* CAN0 error interrupt*/

    .long   CAN0_Tx_Warning_IRQHandler                      /* CAN0 Tx warning interrupt*/

    .long   CAN0_Rx_Warning_IRQHandler                      /* CAN0 Rx warning interrupt*/

    .long   CAN0_Wake_Up_IRQHandler                         /* CAN0 wake up interrupt*/

    .long   SDHC_IRQHandler                                 /* SDHC interrupt*/

    .long   DefaultISR                                      /* 98*/

    .long   DefaultISR                                      /* 99*/

    .long   DefaultISR                                      /* 100*/

    .long   DefaultISR                                      /* 101*/

    .long   DefaultISR                                      /* 102*/

    .long   DefaultISR                                      /* 103*/

    .long   DefaultISR                                      /* 104*/

    .long   DefaultISR                                      /* 105*/

    .long   DefaultISR                                      /* 106*/

    .long   DefaultISR                                      /* 107*/

    .long   DefaultISR                                      /* 108*/

    .long   DefaultISR                                      /* 109*/

    .long   DefaultISR                                      /* 110*/

    .long   DefaultISR                                      /* 111*/

    .long   DefaultISR                                      /* 112*/

    .long   DefaultISR                                      /* 113*/

    .long   DefaultISR                                      /* 114*/

    .long   DefaultISR                                      /* 115*/

    .long   DefaultISR                                      /* 116*/

    .long   DefaultISR                                      /* 117*/

    .long   DefaultISR                                      /* 118*/

    .long   DefaultISR                                      /* 119*/

    .long   DefaultISR                                      /* 120*/

    .long   DefaultISR                                      /* 121*/

    .long   DefaultISR                                      /* 122*/

    .long   DefaultISR                                      /* 123*/

    .long   DefaultISR                                      /* 124*/

    .long   DefaultISR                                      /* 125*/

    .long   DefaultISR                                      /* 126*/

    .long   DefaultISR                                      /* 127*/

    .long   DefaultISR                                      /* 128*/

    .long   DefaultISR                                      /* 129*/

    .long   DefaultISR                                      /* 130*/

    .long   DefaultISR                                      /* 131*/

    .long   DefaultISR                                      /* 132*/

    .long   DefaultISR                                      /* 133*/

    .long   DefaultISR                                      /* 134*/

    .long   DefaultISR                                      /* 135*/

    .long   DefaultISR                                      /* 136*/

    .long   DefaultISR                                      /* 137*/

    .long   DefaultISR                                      /* 138*/

    .long   DefaultISR                                      /* 139*/

    .long   DefaultISR                                      /* 140*/

    .long   DefaultISR                                      /* 141*/

    .long   DefaultISR                                      /* 142*/

    .long   DefaultISR                                      /* 143*/

    .long   DefaultISR                                      /* 144*/

    .long   DefaultISR                                      /* 145*/

    .long   DefaultISR                                      /* 146*/

    .long   DefaultISR                                      /* 147*/

    .long   DefaultISR                                      /* 148*/

    .long   DefaultISR                                      /* 149*/

    .long   DefaultISR                                      /* 150*/

    .long   DefaultISR                                      /* 151*/

    .long   DefaultISR                                      /* 152*/

    .long   DefaultISR                                      /* 153*/

    .long   DefaultISR                                      /* 154*/

    .long   DefaultISR                                      /* 155*/

    .long   DefaultISR                                      /* 156*/

    .long   DefaultISR                                      /* 157*/

    .long   DefaultISR                                      /* 158*/

    .long   DefaultISR                                      /* 159*/

    .long   DefaultISR                                      /* 160*/

    .long   DefaultISR                                      /* 161*/

    .long   DefaultISR                                      /* 162*/

    .long   DefaultISR                                      /* 163*/

    .long   DefaultISR                                      /* 164*/

    .long   DefaultISR                                      /* 165*/

    .long   DefaultISR                                      /* 166*/

    .long   DefaultISR                                      /* 167*/

    .long   DefaultISR                                      /* 168*/

    .long   DefaultISR                                      /* 169*/

    .long   DefaultISR                                      /* 170*/

    .long   DefaultISR                                      /* 171*/

    .long   DefaultISR                                      /* 172*/

    .long   DefaultISR                                      /* 173*/

    .long   DefaultISR                                      /* 174*/

    .long   DefaultISR                                      /* 175*/

    .long   DefaultISR                                      /* 176*/

    .long   DefaultISR                                      /* 177*/

    .long   DefaultISR                                      /* 178*/

    .long   DefaultISR                                      /* 179*/

    .long   DefaultISR                                      /* 180*/

    .long   DefaultISR                                      /* 181*/

    .long   DefaultISR                                      /* 182*/

    .long   DefaultISR                                      /* 183*/

    .long   DefaultISR                                      /* 184*/

    .long   DefaultISR                                      /* 185*/

    .long   DefaultISR                                      /* 186*/

    .long   DefaultISR                                      /* 187*/

    .long   DefaultISR                                      /* 188*/

    .long   DefaultISR                                      /* 189*/

    .long   DefaultISR                                      /* 190*/

    .long   DefaultISR                                      /* 191*/

    .long   DefaultISR                                      /* 192*/

    .long   DefaultISR                                      /* 193*/

    .long   DefaultISR                                      /* 194*/

    .long   DefaultISR                                      /* 195*/

    .long   DefaultISR                                      /* 196*/

    .long   DefaultISR                                      /* 197*/

    .long   DefaultISR                                      /* 198*/

    .long   DefaultISR                                      /* 199*/

    .long   DefaultISR                                      /* 200*/

    .long   DefaultISR                                      /* 201*/

    .long   DefaultISR                                      /* 202*/

    .long   DefaultISR                                      /* 203*/

    .long   DefaultISR                                      /* 204*/

    .long   DefaultISR                                      /* 205*/

    .long   DefaultISR                                      /* 206*/

    .long   DefaultISR                                      /* 207*/

    .long   DefaultISR                                      /* 208*/

    .long   DefaultISR                                      /* 209*/

    .long   DefaultISR                                      /* 210*/

    .long   DefaultISR                                      /* 211*/

    .long   DefaultISR                                      /* 212*/

    .long   DefaultISR                                      /* 213*/

    .long   DefaultISR                                      /* 214*/

    .long   DefaultISR                                      /* 215*/

    .long   DefaultISR                                      /* 216*/

    .long   DefaultISR                                      /* 217*/

    .long   DefaultISR                                      /* 218*/

    .long   DefaultISR                                      /* 219*/

    .long   DefaultISR                                      /* 220*/

    .long   DefaultISR                                      /* 221*/

    .long   DefaultISR                                      /* 222*/

    .long   DefaultISR                                      /* 223*/

    .long   DefaultISR                                      /* 224*/

    .long   DefaultISR                                      /* 225*/

    .long   DefaultISR                                      /* 226*/

    .long   DefaultISR                                      /* 227*/

    .long   DefaultISR                                      /* 228*/

    .long   DefaultISR                                      /* 229*/

    .long   DefaultISR                                      /* 230*/

    .long   DefaultISR                                      /* 231*/

    .long   DefaultISR                                      /* 232*/

    .long   DefaultISR                                      /* 233*/

    .long   DefaultISR                                      /* 234*/

    .long   DefaultISR                                      /* 235*/

    .long   DefaultISR                                      /* 236*/

    .long   DefaultISR                                      /* 237*/

    .long   DefaultISR                                      /* 238*/

    .long   DefaultISR                                      /* 239*/

    .long   DefaultISR                                      /* 240*/

    .long   DefaultISR                                      /* 241*/

    .long   DefaultISR                                      /* 242*/

    .long   DefaultISR                                      /* 243*/

    .long   DefaultISR                                      /* 244*/

    .long   DefaultISR                                      /* 245*/

    .long   DefaultISR                                      /* 246*/

    .long   DefaultISR                                      /* 247*/

    .long   DefaultISR                                      /* 248*/

    .long   DefaultISR                                      /* 249*/

    .long   DefaultISR                                      /* 250*/

    .long   DefaultISR                                      /* 251*/

    .long   DefaultISR                                      /* 252*/

    .long   DefaultISR                                      /* 253*/

    .long   DefaultISR                                      /* 254*/

    .long   0xFFFFFFFF                                      /*  Reserved for user TRIM value*/

    .size    __isr_vector, . - __isr_vector

/* Flash Configuration */

    .section .FlashConfig, "a"

    .long 0xFFFFFFFF

    .long 0xFFFFFFFF

    .long 0xFFFFFFFF

    .long 0x7EFBFFFE

    .equ _NVIC_ICER0, 0xE000E180

    .equ _NVIC_ICPR0, 0xE000E280

    .text

    .thumb

/* Reset Handler */

    .thumb_func

    .align 2

    .globl   Reset_Handler

    .type    Reset_Handler, %function

Reset_Handler:

    cpsid   i               /* Mask interrupts */

    ldr r0, =_NVIC_ICER0    /* Disable interrupts and clear pending flags */

    ldr r1, =_NVIC_ICPR0

    ldr r2, =0xFFFFFFFF

    mov r3, #8

_irq_clear:

    cbz r3, _irq_clear_end

    str r2, [r0], #4        /* NVIC_ICERx - clear enable IRQ register */

    str r2, [r1], #4        /* NVIC_ICPRx - clear pending IRQ register */

    sub r3, r3, #1

    b _irq_clear

_irq_clear_end:

#ifndef __NO_SYSTEM_INIT

    bl SystemInit

#endif

    cpsie   i               /* Unmask interrupts */

/*     Loop to copy data from read only memory to RAM. The ranges

*      of copy from/to are specified by following symbols evaluated in

*      linker script.

*      __etext: End of code section, i.e., begin of data sections to copy from.

*      __data_start__/__data_end__: RAM address range that data should be

*      copied to. Both must be aligned to 4 bytes boundary.  */

    ldr    r1, =__etext

    ldr    r2, =__data_start__

    ldr    r3, =__data_end__

#if 1

/* Here are two copies of loop implemenations. First one favors code size

* and the second one favors performance. Default uses the first one.

* Change to "#if 0" to use the second one */

.LC0:

    cmp     r2, r3

    ittt    lt

    ldrlt   r0, [r1], #4

    strlt   r0, [r2], #4

    blt    .LC0

#else

    subs    r3, r2

    ble    .LC1

.LC0:

    subs    r3, #4

    ldr    r0, [r1, r3]

    str    r0, [r2, r3]

    bgt    .LC0

.LC1:

#endif

#ifdef __STARTUP_CLEAR_BSS

/*     This part of work usually is done in C library startup code. Otherwise,

*     define this macro to enable it in this startup.

*

*     Loop to zero out BSS section, which uses following symbols

*     in linker script:

*      __bss_start__: start of BSS section. Must align to 4

*      __bss_end__: end of BSS section. Must align to 4

*/

    ldr r1, =__bss_start__

    ldr r2, =__bss_end__

    movs    r0, 0

.LC2:

    cmp     r1, r2

    itt    lt

    strlt   r0, [r1], #4

    blt    .LC2

#endif /* __STARTUP_CLEAR_BSS */

#ifndef __START

#define __START _start

#endif

    bl    __START

    .pool

    .size Reset_Handler, . - Reset_Handler

  .align 1

  .thumb_func

  .weak Default_Handler

  .type Default_Handler, %function

Default_Handler:

  b .

  .size Default_Handler, . - Default_Handler

/*    Macro to define default handlers. Default handler

*    will be weak symbol and just dead loops. They can be

*    overwritten by other handlers */

  .macro def_irq_handler handler_name

  .weak \handler_name

  .set \handler_name, Default_Handler

  .endm

/* Exception Handlers */

    def_irq_handler    NMI_Handler

    def_irq_handler    HardFault_Handler

    def_irq_handler    MemManage_Handler

    def_irq_handler    BusFault_Handler

    def_irq_handler    UsageFault_Handler

    def_irq_handler    SVC_Handler

    def_irq_handler    DebugMon_Handler

    def_irq_handler    PendSV_Handler

    def_irq_handler    SysTick_Handler

    def_irq_handler    DMA0_IRQHandler

    def_irq_handler    DMA1_IRQHandler

    def_irq_handler    DMA2_IRQHandler

    def_irq_handler    DMA3_IRQHandler

    def_irq_handler    DMA4_IRQHandler

    def_irq_handler    DMA5_IRQHandler

    def_irq_handler    DMA6_IRQHandler

    def_irq_handler    DMA7_IRQHandler

    def_irq_handler    DMA8_IRQHandler

    def_irq_handler    DMA9_IRQHandler

    def_irq_handler    DMA10_IRQHandler

    def_irq_handler    DMA11_IRQHandler

    def_irq_handler    DMA12_IRQHandler

    def_irq_handler    DMA13_IRQHandler

    def_irq_handler    DMA14_IRQHandler

    def_irq_handler    DMA15_IRQHandler

    def_irq_handler    DMA_Error_IRQHandler

    def_irq_handler    MCM_IRQHandler

    def_irq_handler    FTFE_IRQHandler

    def_irq_handler    Read_Collision_IRQHandler

    def_irq_handler    LVD_LVW_IRQHandler

    def_irq_handler    LLW_IRQHandler

    def_irq_handler    Watchdog_IRQHandler

    def_irq_handler    Reserved39_IRQHandler

    def_irq_handler    I2C0_IRQHandler

    def_irq_handler    I2C1_IRQHandler

    def_irq_handler    SPI0_IRQHandler

    def_irq_handler    SPI1_IRQHandler

    def_irq_handler    I2S0_Tx_IRQHandler

    def_irq_handler    I2S0_Rx_IRQHandler

    def_irq_handler    Reserved46_IRQHandler

    def_irq_handler    UART0_RX_TX_IRQHandler

    def_irq_handler    UART0_ERR_IRQHandler

    def_irq_handler    UART1_RX_TX_IRQHandler

    def_irq_handler    UART1_ERR_IRQHandler

    def_irq_handler    UART2_RX_TX_IRQHandler

    def_irq_handler    UART2_ERR_IRQHandler

    def_irq_handler    UART3_RX_TX_IRQHandler

    def_irq_handler    UART3_ERR_IRQHandler

    def_irq_handler    ADC0_IRQHandler

    def_irq_handler    CMP0_IRQHandler

    def_irq_handler    CMP1_IRQHandler

    def_irq_handler    FTM0_IRQHandler

    def_irq_handler    FTM1_IRQHandler

    def_irq_handler    FTM2_IRQHandler

    def_irq_handler    CMT_IRQHandler

    def_irq_handler    RTC_IRQHandler

    def_irq_handler    RTC_Seconds_IRQHandler

    def_irq_handler    PIT0_IRQHandler

    def_irq_handler    PIT1_IRQHandler

    def_irq_handler    PIT2_IRQHandler

    def_irq_handler    PIT3_IRQHandler

    def_irq_handler    PDB0_IRQHandler

    def_irq_handler    USB0_IRQHandler

    def_irq_handler    USBDCD_IRQHandler

    def_irq_handler    Reserved71_IRQHandler

    def_irq_handler    DAC0_IRQHandler

    def_irq_handler    MCG_IRQHandler

    def_irq_handler    LPTimer_IRQHandler

    def_irq_handler    PORTA_IRQHandler

    def_irq_handler    PORTB_IRQHandler

    def_irq_handler    PORTC_IRQHandler

    def_irq_handler    PORTD_IRQHandler

    def_irq_handler    PORTE_IRQHandler

    def_irq_handler    SWI_IRQHandler

    def_irq_handler    SPI2_IRQHandler

    def_irq_handler    UART4_RX_TX_IRQHandler

    def_irq_handler    UART4_ERR_IRQHandler

    def_irq_handler    UART5_RX_TX_IRQHandler

    def_irq_handler    UART5_ERR_IRQHandler

    def_irq_handler    CMP2_IRQHandler

    def_irq_handler    FTM3_IRQHandler

    def_irq_handler    DAC1_IRQHandler

    def_irq_handler    ADC1_IRQHandler

    def_irq_handler    I2C2_IRQHandler

    def_irq_handler    CAN0_ORed_Message_buffer_IRQHandler

    def_irq_handler    CAN0_Bus_Off_IRQHandler

    def_irq_handler    CAN0_Error_IRQHandler

    def_irq_handler    CAN0_Tx_Warning_IRQHandler

    def_irq_handler    CAN0_Rx_Warning_IRQHandler

    def_irq_handler    CAN0_Wake_Up_IRQHandler

    def_irq_handler    SDHC_IRQHandler

    def_irq_handler    DefaultISR

    .end

/*

** ###################################################################

**     Compilers:           ARM Compiler

**                          Freescale C/C++ for Embedded ARM

**                          GNU C Compiler

**                          GNU C Compiler - CodeSourcery Sourcery G++

**                          IAR ANSI C/C++ Compiler for ARM

**

**     Reference manual:    K22P144M100SF5RM, Rev.2, Apr 2013

**     Version:             rev. 1.7, 2014-02-18

**

**     Abstract:

**         Provides a system configuration function and a global variable that

**         contains the system frequency. It configures the device and initializes

**         the oscillator (PLL) that is part of the microcontroller device.

**

**     Copyright: 2014 Freescale, Inc. All Rights Reserved.

**

**     http:                 www.freescale.com

**     mail:                 support@freescale.com

**

**     Revisions:

**     - rev. 1.0 (2012-06-06)

**         Initial version.

**     - rev. 1.1 (2012-11-12)

**         Update according to reference manual rev.1, draft B

**     - rev. 1.2 (2012-12-04)

**         Update according to reference manual rev.1

**     - rev. 1.3 (2013-03-11)

**         System initialization updated to add 120MHz clock option.

**     - rev. 1.4 (2013-04-05)

**         Changed start of doxygen comment.

**     - rev. 1.5 (2013-05-16)

**         Update according to reference manual rev.2

**     - rev. 1.6 (2013-10-29)

**         Definition of BITBAND macros updated to support peripherals with 32-bit acces disabled.

**         The declaration of clock configurations has been moved to separate header file system_xxxx.h

**         Startup file for gcc has been updated according to CMSIS 3.2.

**         Access restriction of some registers fixed.

**     - rev. 1.7 (2014-02-18)

**         UART0 module - LON registers removed.

**

** ###################################################################

*/

/*!

* @file MK22F12

* @version 1.7

* @date 2014-02-18

* @brief Device specific configuration file for MK22F12 (implementation file)

*

* Provides a system configuration function and a global variable that contains

* the system frequency. It configures the device and initializes the oscillator

* (PLL) that is part of the microcontroller device.

*/

#include <stdint.h>

#include "processor.h"

#if REF_CLK_FREQ == 27000000

#define FRDIV 0x05

#define PRDIV0 0x08

#define VDIV0 0x10

#elif REF_CLK_FREQ == 8000000

#define FRDIV 0x03

#define PRDIV0 0x01

#define VDIV0 0x06

#else

#error Unsupported ref clock freq

#endif

/* ----------------------------------------------------------------------------

   -- SystemInit()

   ---------------------------------------------------------------------------- */

void SystemInit (void) {

#if ((__FPU_PRESENT == 1) && (__FPU_USED == 1))

  SCB->CPACR |= ((3UL << 10*2) | (3UL << 11*2));    /* set CP10, CP11 Full Access */

#endif /* ((__FPU_PRESENT == 1) && (__FPU_USED == 1)) */

  /* Disable the WDOG module */

  /* WDOG_UNLOCK: WDOGUNLOCK=0xC520 */

  WDOG->UNLOCK = WDOG_UNLOCK_WDOGUNLOCK(0xC520); /* Key 1 */

  /* WDOG_UNLOCK: WDOGUNLOCK=0xD928 */

  WDOG->UNLOCK = WDOG_UNLOCK_WDOGUNLOCK(0xD928); /* Key 2 */

  /* WDOG_STCTRLH:

   * ??=0,DISTESTWDOG=0,BYTESEL=0,TESTSEL=0,TESTWDOG=0,??=0,??=1,WAITEN=1,STOPEN=1,DBGEN=0,ALLOWUPDATE=1,WINEN=0,IRQRSTEN=0,CLKSRC=1,WDOGEN=0

   * */

  WDOG->STCTRLH = WDOG_STCTRLH_BYTESEL(0x00) |

      WDOG_STCTRLH_WAITEN_MASK |

      WDOG_STCTRLH_STOPEN_MASK |

      WDOG_STCTRLH_ALLOWUPDATE_MASK |

      WDOG_STCTRLH_CLKSRC_MASK |

      0x0100U;

  /* System clock initialization */

  /* SIM_CLKDIV1:

   * OUTDIV1=0,OUTDIV2=1,OUTDIV3=3,OUTDIV4=3,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0

   * */

  SIM->CLKDIV1 = SIM_CLKDIV1_OUTDIV1(0x00) | SIM_CLKDIV1_OUTDIV2(0x01) | SIM_CLKDIV1_OUTDIV3(0x03) | SIM_CLKDIV1_OUTDIV4(0x03); /* Set the system prescalers to safe value */

  /* SIM_SCGC5: PORTA=1 */

  SIM->SCGC5 |= SIM_SCGC5_PORTA_MASK;   /* Enable clock gate for ports to enable pin routing */

  if ((PMC->REGSC & PMC_REGSC_ACKISO_MASK) != 0x0U) {

      /* PMC_REGSC:

       * ACKISO=1 */

      PMC->REGSC |= PMC_REGSC_ACKISO_MASK; /* Release IO pads after wakeup from VLLS mode. */

  }

  /* SIM_CLKDIV1:

   * OUTDIV1=0,OUTDIV2=1,OUTDIV3=1,OUTDIV4=4,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0

   * */

  SIM->CLKDIV1 = SIM_CLKDIV1_OUTDIV1(0x00) | SIM_CLKDIV1_OUTDIV2(0x01) | SIM_CLKDIV1_OUTDIV3(0x01) | SIM_CLKDIV1_OUTDIV4(0x04); /* Update system prescalers */

  /* SIM_SOPT2: PLLFLLSEL=1

   * */

  SIM->SOPT2 |= SIM_SOPT2_PLLFLLSEL_MASK; /* Select PLL as a clock source for various peripherals */

  /* SIM_SOPT1:

   * OSC32KSEL=3 */

  SIM->SOPT1 |= SIM_SOPT1_OSC32KSEL(0x03); /* LPO 1kHz oscillator drives 32 kHz clock for various peripherals */

  /* Switch to FBE

   * Mode */

  /* MCG_C2:

   * LOCRE0=0,??=0,RANGE0=2,HGO0=0,EREFS0=1,LP=0,IRCS=0

   * */

  MCG->C2 = (MCG_C2_RANGE0(0x02) | MCG_C2_EREFS0_MASK);

  /* OSC_CR:

   * ERCLKEN=1,??=0,EREFSTEN=0,??=0,SC2P=0,SC4P=0,SC8P=0,SC16P=0

   * */

  OSC->CR = OSC_CR_ERCLKEN_MASK;

  /* MCG_C7:

   * OSCSEL=0 */

  MCG->C7 &= (uint8_t)~(uint8_t)(MCG_C7_OSCSEL_MASK);

  /* MCG_C1:

   * CLKS=2,FRDIV=5,IREFS=0,IRCLKEN=1,IREFSTEN=0

   * */

  MCG->C1 = (MCG_C1_CLKS(0x02) | MCG_C1_FRDIV(FRDIV) | MCG_C1_IRCLKEN_MASK);

  /* MCG_C4:

   * DMX32=0,DRST_DRS=0

   * */

  MCG->C4 &= (uint8_t)~(uint8_t)((MCG_C4_DMX32_MASK | MCG_C4_DRST_DRS(0x03)));

  /* MCG_C5:

   * ??=0,PLLCLKEN0=0,PLLSTEN0=0,PRDIV0=8

   * */

  MCG->C5 = MCG_C5_PRDIV0(PRDIV0);

  /* MCG_C6:

   * LOLIE0=0,PLLS=0,CME0=0,VDIV0=0x10

   * */

  MCG->C6 = MCG_C6_VDIV0(VDIV0);

  while((MCG->S & MCG_S_OSCINIT0_MASK) == 0x00U) { /* Check that the oscillator is running */

  }

  while((MCG->S & MCG_S_IREFST_MASK) != 0x00U) { /* Check that the source of the FLL reference clock is the external reference clock. */

  }

  while((MCG->S & 0x0CU) != 0x08U) {    /* Wait until external reference clock is selected as MCG output */

  }

  /* Switch to PBE Mode */

  /* MCG_C6: LOLIE0=0,PLLS=1,CME0=0,VDIV0=0x10 */

  MCG->C6 = (MCG_C6_PLLS_MASK | MCG_C6_VDIV0(VDIV0));

  while((MCG->S & 0x0CU) != 0x08U) {    /* Wait until external reference clock is selected as MCG output */

  }

  while((MCG->S & MCG_S_LOCK0_MASK) == 0x00U) { /* Wait until locked */

  }

  /* Switch to PEE Mode */

  /* MCG_C1: CLKS=0,FRDIV=5,IREFS=0,IRCLKEN=1,IREFSTEN=0 */

  MCG->C1 = (MCG_C1_CLKS(0x00) | MCG_C1_FRDIV(FRDIV) | MCG_C1_IRCLKEN_MASK);

  while((MCG->S & 0x0CU) != 0x0CU) {    /* Wait until output of the PLL is selected */

  }

}

0 项奖励
回复

2,948 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Aaron Ledger,

Thanks for the information! I have passed the above to our expert team for a review, and will let you know if I have any feedback.

Thanks for your patience!

Kan

0 项奖励
回复