Which method use to drive String of LED of type WS2811?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which method use to drive String of LED of type WS2811?

2,145 Views
arnogir
Senior Contributor II

Hello,

I'm investigating about how drive a string of this type of LED:

https://cdn-shop.adafruit.com/datasheets/WS2812.pdf

These LED are driven is "Serial" RGB data.

But this could up to 800Khz.

Is any body has already drive this LED with a Kinetis (For me a K60 under MQX 4.2)?

Which method could be beter?

(Gpio, SPI, other??)

With/Without DMA?

The aim is to have CPU charge lower has possible!..

Thank

0 Kudos
Reply
2 Replies

1,989 Views
BlackNight
NXP Employee
NXP Employee
0 Kudos
Reply

1,989 Views
arnogir
Senior Contributor II

Hello

I will try with the first exemple (My Target K60 not have FlexIO)

I must adapt tis with my plateforme (MQX 4.2 on K60)

Thank

0 Kudos
Reply