Which Kinetics MCUs come with ROM Bootloaders?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which Kinetics MCUs come with ROM Bootloaders?

2,916 Views
jeremyanderson
Contributor III

This question was asked and answered three years ago, but the link is stale and just lands me on a useless front page.  Specifically, if I populate my design with a K66 MCU, will there be a ROM bootloader already there?  If so, where is the documentation for using this to bootstrap my system?

Tags (1)
2 Replies

2,626 Views
adriancano
NXP Employee
NXP Employee

These are the device families supporting MCUBOOT in ROM

K27
K28
K27
K80
K81
K82
KE14F
KE14Z
KE15Z
KE16F
KE16F
KE18F
KL03
KL03
KL13
KL17
KL27
KL28
KL33
KL43
KL81
KL82

Regards

2,626 Views
mjbcswitzerland
Specialist V

Hi Jeremy

Here is a (possibly incomplete) list of parts containing the ROM loader today:
KL03
KL17
KL27
KL28
KL43
KL82
KE15

The K66 doesn't have one but you can load a "serial loader" (see links below) for:
- USB-MSD or USB-CDC device
- SD card or Memory stick
- KBOOT UART
- KBOOT USB-HID
- AN2295 UART
- SREC/iHex UART
- Modbus slave
- I2C slave
- Ethernet web server


Regards

Mark


Kinetis: http://www.utasker.com/kinetis.html
Kinetis K66:
- http://www.utasker.com/kinetis/TWR-K65F180M.html
- http://www.utasker.com/kinetis/FRDM-K66F.html
- http://www.utasker.com/kinetis/TEENSY_3.6.html

K66 Serial loader: http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.pdf


Free Open Source solution: https://github.com/uTasker/uTasker-Kinetis
Working project in 15 minutes video: https://youtu.be/K8ScSgpgQ6M

For better, faster, cheaper product developments consider the uTasker developer's version, professional Kinetis support, one-on-one training and complete fast-track project solutions to set you apart from the herd : http://www.utasker.com/support.html