Where is the comparator input?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is the comparator input?

Jump to solution
2,133 Views
pietrodicastri
Senior Contributor II

Good morning

I read on the Figure 36-1 of the RM for the K60 the two comparator's input selectable through VRSEL are Vin1 and Vin2.

In my understanding should be somewhere in the pinout of the uC. I don't find.

Maybe there is a good reason why are not there....

Thank You

Tags (3)
1 Solution
1,992 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Pietro,

There is more info regarding Vin1 and Vin2 in Chapter 3, please kindly refer to the following for details.

1.png

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,993 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Pietro,

There is more info regarding Vin1 and Vin2 in Chapter 3, please kindly refer to the following for details.

1.png

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,992 Views
pietrodicastri
Senior Contributor II

Yes

Thank You

0 Kudos
Reply