What will be the extreme values of ADC result when resolution is 16 bit?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What will be the extreme values of ADC result when resolution is 16 bit?

1,080件の閲覧回数
pramodk_g_
Contributor III

Hi everyone,

                                 When I  run ADC example for TWR K60D100M , it is found that adc result is 32267 when probed to 3.3V and 65523 or 34 etc. for 0v . Adc resolution used in the code is 16bit, so the extreme value should be 65535 and 0 (For 3.3V and 0V ), is it correct?. Is there any change need to achieve this or I went wrong somewhere?

Please help..

Thanks

Pramod

タグ(4)
0 件の賞賛
返信
1 返信

859件の閲覧回数
hectorsanchez
Contributor IV

Hi Pramod,

I suggest you to check this thread: Re: ADC on TWRK60N512 ?
Keep me informed if this helped you.

Best Regards,

Hector Sanchez

0 件の賞賛
返信