What is the difference between Core Clock and Bus Clock ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the difference between Core Clock and Bus Clock ?

3,132 Views
sivakumarananth
Contributor I

What is the difference between Core Clock and Bus Clock ?

Labels (1)
0 Kudos
Reply
1 Reply

2,523 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Siva Kumar Anantharaman,

The core clock is used to drive the ARM cortex-m core, while bus clock is used by the bus slaves and peripherals. In most cases for Kinetis part, the max bus clock is half of the max core clock, but for special case such as 50MHz part, they can be the same. Please refer to the chaper 5 "Clock Distribution" for more details.

result.png

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply