What is the difference between Core Clock and Bus Clock ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the difference between Core Clock and Bus Clock ?

3,121件の閲覧回数
sivakumarananth
Contributor I

What is the difference between Core Clock and Bus Clock ?

ラベル(1)
0 件の賞賛
返信
1 返信

2,512件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Siva Kumar Anantharaman,

The core clock is used to drive the ARM cortex-m core, while bus clock is used by the bus slaves and peripherals. In most cases for Kinetis part, the max bus clock is half of the max core clock, but for special case such as 50MHz part, they can be the same. Please refer to the chaper 5 "Clock Distribution" for more details.

result.png

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信