Sounds good, we're very interested in this product now, probably will get the tower system module.
Anyway, I was able to create the remaining independent PWM signals with PIT!
Quick question: what's the difference in using DMA with other modules instead of just using the modules themselves because I've seen a few application notes that demonstrate that approach, such as PIT with DMA, SPI with DMA, and so on. Is the TWR-MEM module required to use DMA?
One final question, is there a wireless or bluetooth module for the K60 or the KV58? Something you can add on to the tower?
Thanks!