What is the KL17 temperature slope value?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the KL17 temperature slope value?

1,707件の閲覧回数
tonymakkiel
Contributor III

Hi,

What are the cold and hot temperature slope value for KL17 mentioned in the reference manual (23.5.8)?  In the example code (adc_low_power_twrkl43z48m) a different equation seem to be used.

Temperature = 25 - (ADCR_T - ADCR_TEMP25) * 100 / ADCR_100M

The above equation will always return negative value.  Should it be

Temperature = 25 - ((ADCR_T - ADCR_TEMP25) / ADCR_100M)

?

Many Thanks,

Tony

3 返答(返信)

1,542件の閲覧回数
egoodii
Senior Contributor III

You might want to refer to my posts on temperature-calculation, including:

https://community.nxp.com/thread/390524 

1,542件の閲覧回数
tonymakkiel
Contributor III

Thank you.

0 件の賞賛
返信

1,542件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

You can find the Temp sensor slope on the data sheet, please also use the AN3031 for reference

Data sheet

AN3031

Regards

Vicente Gomez

0 件の賞賛
返信