What is a flashrom cycle? MKM34Z256

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is a flashrom cycle? MKM34Z256

ソリューションへジャンプ
2,481件の閲覧回数
zunda1958
Contributor II

Please let me know.


The following table describes the endurance of the FLASHROM of the MKM34Z256VLL7 in the KM series.
Data Sheet 3.3.1.4 Reliability Specifications Table 27. NVM Reliability Specifications
Does "cycle endurance" mean the number of times a sector (2KB) can be erased?
Do you mean the maximum number of times a sector can be erased, for example, if one sector is erased and written 64 bytes at a time?

Thank you in advance.

0 件の賞賛
返信
1 解決策
2,435件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that the erasing operation make the bits of flash data from 0 to 1, and the original 1 remains 1, in other words, after erasing, the flash data will be all 1, it means that the flash will be 0xFF, 0xFF...after erasing.

The programming will make the 1 to 0, if the data bits you write is 1, the 1 will keep. The flash programming can not make bit from 0 to 1.

In conclusion, for flash operation, before you program a flash page, sector, you have to erase the page, sector, then program it. In other words, one erase operation, one programming operation. It is impossible that one erasing operation and multiple programming happen.

Because of one erasing and one programming operation, so one erasing/programming cycle is counted as 1 cycle.

Hope it can help you

BR

XiangJun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,454件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As the note 2 says "Cycling endurance represents number of program/erase cycles at -40 °C ≤ Tj ≤ 125 °C.", one erasing/programming ia called one cycle endurance, the flash  Cycling endurance is 50 K typically.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信
2,439件の閲覧回数
zunda1958
Contributor II

Sorry for the repetition.


You mean the program/erase cycle is the number of erases per sector, right?
For example, if the number of program/erase cycles is n (n = 1,000), then each sector can be erased n times, and furthermore, if a 2 KB sector is erased after 4 bytes are written to different addresses 512 times, then the number of program/erase cycles is counted as 1. Is it correct to say that the number of erase cycles counts as one?


Thank you in advance.

 

0 件の賞賛
返信
2,436件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that the erasing operation make the bits of flash data from 0 to 1, and the original 1 remains 1, in other words, after erasing, the flash data will be all 1, it means that the flash will be 0xFF, 0xFF...after erasing.

The programming will make the 1 to 0, if the data bits you write is 1, the 1 will keep. The flash programming can not make bit from 0 to 1.

In conclusion, for flash operation, before you program a flash page, sector, you have to erase the page, sector, then program it. In other words, one erase operation, one programming operation. It is impossible that one erasing operation and multiple programming happen.

Because of one erasing and one programming operation, so one erasing/programming cycle is counted as 1 cycle.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信