What is FTM FAULT?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,181件の閲覧回数
jurijs_jonass
Contributor I

Hi, Colleagues!

I can not find more or less logical description about FTM FAULT condition. Anybody know, what is understood under FAULT condition of the FTM?

Thanks in advance, Jurijs

タグ(2)
1 解決策
2,909件の閲覧回数
eduardo_viramon
NXP Employee
NXP Employee

Jurijs,

FTM fault is a feature used by FTM to automatically shut down PWM outputs when the fault pins become asserted (set or cleared).

This feature is important in control applications where if a fault occurs (over current, over temperature, etc.) the outputs can be automatically and quickly disabled to avoid damaging the hardware or other catastrophic events.

For specific details on how it works and how to configure faults (there are many modes), you can consult the ref manual:

http://cache.freescale.com/files/32bit/doc/ref_manual/K40P100M100SF2V2RM.pdf?fpsp=1

Page: 914, or the fault control section of the FTM chapter of the specific Kinetis device you are using.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,910件の閲覧回数
eduardo_viramon
NXP Employee
NXP Employee

Jurijs,

FTM fault is a feature used by FTM to automatically shut down PWM outputs when the fault pins become asserted (set or cleared).

This feature is important in control applications where if a fault occurs (over current, over temperature, etc.) the outputs can be automatically and quickly disabled to avoid damaging the hardware or other catastrophic events.

For specific details on how it works and how to configure faults (there are many modes), you can consult the ref manual:

http://cache.freescale.com/files/32bit/doc/ref_manual/K40P100M100SF2V2RM.pdf?fpsp=1

Page: 914, or the fault control section of the FTM chapter of the specific Kinetis device you are using.

0 件の賞賛
返信
2,909件の閲覧回数
jurijs_jonass
Contributor I

Thanks a lot!!!

:smileywink: