What is FTM FAULT?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What is FTM FAULT?

跳至解决方案
3,174 次查看
jurijs_jonass
Contributor I

Hi, Colleagues!

I can not find more or less logical description about FTM FAULT condition. Anybody know, what is understood under FAULT condition of the FTM?

Thanks in advance, Jurijs

标记 (2)
1 解答
2,902 次查看
eduardo_viramon
NXP Employee
NXP Employee

Jurijs,

FTM fault is a feature used by FTM to automatically shut down PWM outputs when the fault pins become asserted (set or cleared).

This feature is important in control applications where if a fault occurs (over current, over temperature, etc.) the outputs can be automatically and quickly disabled to avoid damaging the hardware or other catastrophic events.

For specific details on how it works and how to configure faults (there are many modes), you can consult the ref manual:

http://cache.freescale.com/files/32bit/doc/ref_manual/K40P100M100SF2V2RM.pdf?fpsp=1

Page: 914, or the fault control section of the FTM chapter of the specific Kinetis device you are using.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,903 次查看
eduardo_viramon
NXP Employee
NXP Employee

Jurijs,

FTM fault is a feature used by FTM to automatically shut down PWM outputs when the fault pins become asserted (set or cleared).

This feature is important in control applications where if a fault occurs (over current, over temperature, etc.) the outputs can be automatically and quickly disabled to avoid damaging the hardware or other catastrophic events.

For specific details on how it works and how to configure faults (there are many modes), you can consult the ref manual:

http://cache.freescale.com/files/32bit/doc/ref_manual/K40P100M100SF2V2RM.pdf?fpsp=1

Page: 914, or the fault control section of the FTM chapter of the specific Kinetis device you are using.

0 项奖励
回复
2,902 次查看
jurijs_jonass
Contributor I

Thanks a lot!!!

:smileywink: