What is FTM FAULT?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is FTM FAULT?

Jump to solution
3,114 Views
jurijs_jonass
Contributor I

Hi, Colleagues!

I can not find more or less logical description about FTM FAULT condition. Anybody know, what is understood under FAULT condition of the FTM?

Thanks in advance, Jurijs

Tags (2)
1 Solution
2,842 Views
eduardo_viramon
NXP Employee
NXP Employee

Jurijs,

FTM fault is a feature used by FTM to automatically shut down PWM outputs when the fault pins become asserted (set or cleared).

This feature is important in control applications where if a fault occurs (over current, over temperature, etc.) the outputs can be automatically and quickly disabled to avoid damaging the hardware or other catastrophic events.

For specific details on how it works and how to configure faults (there are many modes), you can consult the ref manual:

http://cache.freescale.com/files/32bit/doc/ref_manual/K40P100M100SF2V2RM.pdf?fpsp=1

Page: 914, or the fault control section of the FTM chapter of the specific Kinetis device you are using.

View solution in original post

0 Kudos
Reply
2 Replies
2,843 Views
eduardo_viramon
NXP Employee
NXP Employee

Jurijs,

FTM fault is a feature used by FTM to automatically shut down PWM outputs when the fault pins become asserted (set or cleared).

This feature is important in control applications where if a fault occurs (over current, over temperature, etc.) the outputs can be automatically and quickly disabled to avoid damaging the hardware or other catastrophic events.

For specific details on how it works and how to configure faults (there are many modes), you can consult the ref manual:

http://cache.freescale.com/files/32bit/doc/ref_manual/K40P100M100SF2V2RM.pdf?fpsp=1

Page: 914, or the fault control section of the FTM chapter of the specific Kinetis device you are using.

0 Kudos
Reply
2,842 Views
jurijs_jonass
Contributor I

Thanks a lot!!!

:smileywink: