What difference between K60 and K63/K64 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What difference between K60 and K63/K64 ?

5,906 Views
lucky06200
Contributor II

Hello,

How is compatibility between K60 and K63/K64 processor?

Is there comparison somewhere?

Some idea?

I use K60N512ZVLQ10 and i search more comfortable RAM and ROM memory size.

Tags (3)
0 Kudos
Reply
7 Replies

4,019 Views
anthony_huereca
NXP Employee
NXP Employee

The biggest difference is that K63 and K64 are part of the new second generation Kinetis K devices (K2). Beyond what Mark and Justin posted, one of the other new features is crystal-less USB capabilities to save on BOM costs. Also there are also power and cost savings available with K2 parts depending on the devices selected.

There's also a ton of new enablement rolling out alongside these K2 devices:

Kinetis Software Development Kit (KSDK): KINETIS_SDK: Software Development Kit for Kinetis MCUs

Kinetis Bootloader: KBOOT: Kinetis Bootloader

Kinetis Design Studio (KDS): KDS_IDE: Kinetis Design Studio Integrated Development Environment (IDE)

0 Kudos
Reply

4,019 Views
kai_liu
Senior Contributor I

nice, do they support L as well?

0 Kudos
Reply

4,019 Views
anthony_huereca
NXP Employee
NXP Employee

The bootloader and Kinetis Development Studio (KDS) already support some KL devices currently. Other devices will be added further down the line. The new K2 devices will be first along with other newly released Kinetis parts, and then over time select older Kinetis devices will be added as well.

0 Kudos
Reply

4,019 Views
justinbmortimer
NXP Employee
NXP Employee

That's a great question!  I would recommend checking out the K6x family fact sheet to get a good perspective on these families.  Also, expanding on what Mark provided, here's a high level summary of the product families:

  • K60 :High Mixed Signal Integration
  • K61 : High Mixed Signal Integration w/ tamper detection
  • K64 : High SRAM
  • K63 : High SRAM w/ tamper detection

Regards, Justin

0 Kudos
Reply

4,019 Views
williamely
Contributor IV

I'd like to know the answer to this also.

From what I can tell the K63/4 have an FPU but no NFC.

The K63/64 only have 120 MHz chips.

The K64 seems to be pin-pin compatible with K60.

I'm not sure what the difference is between the K63 and K64.

0 Kudos
Reply

4,019 Views
cfgmgr
Contributor III

I think k64 has only CAN0 (no CAN1)

0 Kudos
Reply

4,019 Views
mjbcswitzerland
Specialist V

Hi

I would say that these are the main differences between K60, K63 and K64 (120Meg parts) are:

- K63 and K64 have more memory (up to 1Meg Flash / 260k RAM)

- K63 and K64 have no TSI

- K64 has no tamper

- K63 and K64 have CAN0 but not CAN1

Regards

Mark

0 Kudos
Reply