jeremyzhou
		
			jeremyzhou
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Michael,
Please download the sample code of the TWR-K70 through the link as below.
Hope this helps!
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks. I will go through these, but I'm still not sure which sample code from which directory it is that is running on the TWR-K70. It lights the leds when you tip the accelerometer on the board at different angles. I'd like to know this before I erase the board's flash and can't put it back to the default state.
Mike