What are changes we need to made to port the code from k60 to k66

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What are changes we need to made to port the code from k60 to k66

3,149 次查看
maheshwarreddy
Contributor I

hi,

    The Ethernet works fine in k60 ,But now we replaced k60 with k66, the same code is not  working in k66 the interrupts are also not occurring , Any changes we needs to do for initialization part

标签 (1)
标记 (2)
0 项奖励
回复
10 回复数

2,848 次查看
maheshwarreddy
Contributor I

ksdk2.0 I snot downloading properly and also the ksdk1.0 is also not downloading . After downloading it is saying corrupted or invalied.

0 项奖励
回复

2,848 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi maheshwar reddy,

I've already uploaded the KSDK 2.0 and please have a try.

SDK_2.0_FRDM-K66F.zip - Google Drive
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,848 次查看
maheshwarreddy
Contributor I

can you check my code of Ethernet part.

0 项奖励
回复

2,848 次查看
maheshwarreddy
Contributor I

But in wire shark also nothing is coming,

0 项奖励
回复

2,848 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi maheshwar reddy,

Thanks for your reply.

As mentioned before, the

According to the previous statement, KSDK has provided the Ethernet demos, you refer to them for details and install the KSDK by following the thread How to: install KSDK 2.0 .

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,848 次查看
maheshwarreddy
Contributor I

it is not downloading ....after downloading it is saying file corrupted

0 项奖励
回复

2,848 次查看
maheshwarreddy
Contributor I

I had changed the interrupt values also , iam I had used the wireshark  to receive the Ethernet packet for k60 board ,even thought the Ethernet in k66 is not working

0 项奖励
回复

2,848 次查看
maheshwarreddy
Contributor I

Iam using keil5, We are giving external clock on EXTAL( pin.no 72) for both phy(lan8710 in RMII mode) and processor but we are not getting any interrupts .

0 项奖励
回复

2,848 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi maheshwar reddy,

Thanks for your reply.

I'd like to know whether you had already used the Wireshark to capture the packet or not.

After compare the captured the packet, we can figure out the difference of ethernet application between the K60 and the K60.

And I think I miss one thing, the ethernet related interrupt vectors are different between the K60 and K66.

pastedImage_1.png

                                                                                    Fig K60

pastedImage_2.png

                                                                                        Fig K66

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,848 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi maheshwar reddy,

The Ethernet module is almost identical for all Kinetis parts except for the Ethernet clocking configuration.

I'd highly recommend you to refer to the Ethernet demos which are from the KSDK and you can install the KSDK by following the thread How to: install KSDK 2.0 .
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复