Watchdog not enabled on startup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Watchdog not enabled on startup

ソリューションへジャンプ
2,753件の閲覧回数
justusandjustic
Contributor III

I have a program that uses Processor Expert and it appears as if the watchdog is not functioning.  I have added a WatchDog component to my project, but have disabled auto initialization.  I have also gone into the 'Cpu:SKEAZN...' processor component and set 'Watchdog disable' to 'no'.  My assumption is that this should leave the watchdog registers as their default values (which should be enabled, and set to some reset time), since the Watchdog component never initializes itself.  However, when I run the program, it is not resetting on watchdog timeout.  Clearly I am not understanding something here; what am I missing?

-Josiah

ラベル(1)
0 件の賞賛
返信
1 解決策
2,249件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Josiah,

The watchdog may be disabled in __init_hardware(). Please check the code:

disable WDOG.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,250件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Josiah,

The watchdog may be disabled in __init_hardware(). Please check the code:

disable WDOG.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,249件の閲覧回数
justusandjustic
Contributor III

It looks like that was indeed the problem.  I thought I took care of that when I changed the Cpu component settings to 'Watchdog disable: no', but it looks like adding a WatchDog components also inserts that same code to disable the watchdog in __init_hardware(). 

My plan now is the modify the watchdog registers within the __init_hardware() function instead of using a watchdog component, to make sure that the watchdog is never disabled after startup.  I put my watchdog initialization code in the "User code before PE initialization" property of the Cpu component.  Any reason why this might be a bad way to do this?

watchdog.png

-Josiah

0 件の賞賛
返信