Wake-up from LLS using a non-LLWU pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wake-up from LLS using a non-LLWU pin

ソリューションへジャンプ
1,885件の閲覧回数
javervalino
Contributor III

Hello all,

I just want to know if its possible for a KL15 mcu to wakeup from lls using a non-llwu pin. In our case we use PTA4 (a NMI pin) as an interrupt source, this supposed to wakeup the unit from lls.

Thank you very much.

Regards,

Javer

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 解決策
1,776件の閲覧回数
santiago_lopez
NXP Employee
NXP Employee

Hi Javier,

According to the KL15 Reference Manual on Chapter 3.4.4.2, the microcontroller can wakeup using the NMI when the pin is enabled and asserted

http://cache.freescale.com/files/32bit/doc/ref_manual/KL15P80M48SF0RM.pdf?fasp=1&WT_TYPE=Reference%2...

Remember that the NMI pin must be selected in the PORTA_PCR4 mux and the NMI interrupt enabled in the FOPT register.

Saludos

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,777件の閲覧回数
santiago_lopez
NXP Employee
NXP Employee

Hi Javier,

According to the KL15 Reference Manual on Chapter 3.4.4.2, the microcontroller can wakeup using the NMI when the pin is enabled and asserted

http://cache.freescale.com/files/32bit/doc/ref_manual/KL15P80M48SF0RM.pdf?fasp=1&WT_TYPE=Reference%2...

Remember that the NMI pin must be selected in the PORTA_PCR4 mux and the NMI interrupt enabled in the FOPT register.

Saludos

0 件の賞賛
返信