Vary frequency of pwm in KEA-128?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vary frequency of pwm in KEA-128?

943件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi,

    I want to vary the frequency of pwm inKEA-128. I am using output compare mode and I want to vary PWM frequency between 300 Hz to 400 Hz, How do I do it, Can you give me any example for this?

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

764件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The FTMx_MOD can be used to vary frequency of pwm.
If you are using Processor Expert with KDS3.2 , the PPG_LDD can be used to realize it.
Or you can refer the method of it.

PPG_LDD SetFrequencyHz.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信