Vary frequency of pwm in KEA-128?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Vary frequency of pwm in KEA-128?

999 次查看
vigneshbalaji
Senior Contributor I

Hi,

    I want to vary the frequency of pwm inKEA-128. I am using output compare mode and I want to vary PWM frequency between 300 Hz to 400 Hz, How do I do it, Can you give me any example for this?

标记 (2)
0 项奖励
回复
1 回复

820 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The FTMx_MOD can be used to vary frequency of pwm.
If you are using Processor Expert with KDS3.2 , the PPG_LDD can be used to realize it.
Or you can refer the method of it.

PPG_LDD SetFrequencyHz.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

0 项奖励
回复