VLQ100 MCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,402件の閲覧回数
gsanchez
Contributor III

Hi all, I'm trying to start programming a custom board, that have a PK60N512 VLQ100 MCU. Where I can found the update package for that distribution pins for use with Processor Expert?

Thanks.

0 件の賞賛
返信
1 解決策
2,246件の閲覧回数
admin
Specialist II

Freescale changed the format of the Kinetis part number when the part went to production. The PK series are pre-production parts.  The MK60DN512ZVLQ10 is the functional equivalent to your part.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,246件の閲覧回数
ProcessorExpert
Senior Contributor III

Hello,

 

I use latest version of CW V10.2 + update and I have not encountered a problem with selection of such package. Could you please specify what version do you use?

 

Donwload page:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&fpsp=1&tab=Design_Tools_Tab

 

best regards
Vojtech Filip
Processor Expert Support Team

0 件の賞賛
返信
2,246件の閲覧回数
gsanchez
Contributor III

Thanks for your answer.

 

I'm using:

- CodeWarrior for MCU
Version: 10.2
Build Id:120126

 

And when I want to choose the device package (Project -> Change device/Connection), the only packages that I can select are (in Kinetis K60):

MK60DN512ZVLQ10 144 pins LQFP

MK60DN512ZVMD10 144 pins MAPBGA

MK60DN512ZVMC10 121 pins MAPBGA

MK60DN512ZVLL10 100 pins LQFP

 

And my device package is PK60N512 VLQ100. So, where I can found it? Or I can use another to replace it?

 

Thanks.

0 件の賞賛
返信
2,247件の閲覧回数
admin
Specialist II

Freescale changed the format of the Kinetis part number when the part went to production. The PK series are pre-production parts.  The MK60DN512ZVLQ10 is the functional equivalent to your part.

0 件の賞賛
返信