Using the Internal FLASH for store data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using the Internal FLASH for store data

2,155件の閲覧回数
alicetin
Contributor I

Hello,

I want to store any data in my Kinetis MCU's(MKV11Z) flash. I want to read last data value when mcu turn on. There are good pages like Erich Styger's Blog . I read it but I can't try code. Because  I couldnt acces component inspector page at MCUXpresso. 

Are there any way to store data in kinetis MCU? or example?

Thanks for the helps.

Ali Bugra Cetin

タグ(5)
0 件の賞賛
返信
1 返信

2,147件の閲覧回数
ErichStyger
Specialist I

Hi @alicetin ,

I'm using the same (well, similar) approach with the McuLib which includes basically many of the former Processor Expert component functionality, but now ported to the MCUXpresso SDK.

You might have a read at:

https://mcuoneclipse.com/2021/12/19/key-value-pairs-in-flash-memory-file-system-less-minini/

I'm using it with an LPC55S16 here too:

https://mcuoneclipse.com/2021/12/30/lorawan-with-nxp-lpc55s16-and-arm-cortex-m33/

The key part is in the McuFlash.c

ErichStyger_0-1673509067385.png

It supports 'Kinetis', but I have used it only with the K22 and K02 family, and I don't have any KV one. So I assume you would have to implement the basic flash programming in McuFlash.c/h/config, but this should not be difficult (I hope).

I hope this helps,

Erich

0 件の賞賛
返信