Using the FRDM-HB2000-EVM evaluation board with a function generator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using the FRDM-HB2000-EVM evaluation board with a function generator

1,598件の閲覧回数
carterhough
Contributor I

I recently purchased the FRDM-HB2000-EVM evaluation board to use for a customer demo. On page 19 of the User's guide (Doc. #: KTFRDMHB2000EVM), it illustrates the hardware configuration for using this board with a function generator rather than the FRDM-KL25Z board and SPIGen interface. I followed the setup instructions, but am receiving a 'Status Fault' and cannot seem to figure out how to activate the output. 

Note: I configured the board with the FRDM-KL25Z board and SPIGen interface and everything works fine.

Is there any additional documentation on configuring this board with the function generator?

0 件の賞賛
返信
1 返信

1,390件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

For your case, did you install the SPI H-Bridge driver based on HB2000 and HB2001: http://www.nxp.com/files/analog/doc/user_guide/HB2000-HB2001SWUG.pdf.

0 件の賞賛
返信