Is Kinetis K66 series a drop in replacement for K64

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is Kinetis K66 series a drop in replacement for K64

跳至解决方案
1,230 次查看
geovarghese
Contributor II

Hi,

We are using MK64FN1M0VMD12 in one of our design. We would like to upgrade to the K66 series. Not so much for the memory but for the speed as it is 50% faster and it also has crypto engine if in the future we need to secure the LAN communication.  If we are to do this ideally it would have to be drop in replacement for hardware and code or I end up with different models that are not compatible. Can any one please confirm whether MK66FN2M0VMD18 can be used as a direct replacement in our case.

Regards,

Geo

0 项奖励
回复
1 解答
1,086 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Geo,

Definitely, the MK66FN2M0VMD18 can replace the MK64FN1M0VMD12 directly.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,087 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Geo,

Definitely, the MK66FN2M0VMD18 can replace the MK64FN1M0VMD12 directly.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复